This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM6442: ICSSG0 MII doesn't work in SDK9.1.0.8

Part Number: AM6442
Other Parts Discussed in Thread: AM6422, TMDS64EVM, DP83620

With same configuration and same board, the icssg0 two MII ports don't work with SDK9.1, it can detect PHY link, but can't ping through. the same board can work with SDK8.6. 

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/AM6422_2D00_20240108.syscfg

https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/791/k3_2D00_am642_2D00_evm.dts

ATT94523.config

U-Boot SPL 2021.01-00001-g1babd0e42c-dirty (Oct 18 2023 - 17:34:15 +0800)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed 1
Resetting on cold boot to workaround ErrataID:i2331
resetting ...

U-Boot SPL 2021.01-00001-g1babd0e42c-dirty (Oct 18 2023 - 17:34:15 +0800)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed 1
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
#SPL initial stack usage: 13424 bytes #
SPL malloc() before relocation used 0x1f58 bytes (7 KB)
>>SPL: board_init_r()
spl_init
Trying to boot from MMC1
Authentication passed
Authentication passed
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Warning: Did not detect image signing certificate. Skipping authentication to prevent boot failure. This will fail on Security Enforcing(HS-SE) devices
Unsupported OS image.. Jumping nevertheless..
loaded - jumping to U-Boot...
init_env from device 9 not supported!
Starting ATF on ARM64 core...

NOTICE:  BL31: v2.8(release):v2.8-226-g2fcd408bb3-dirty
NOTICE:  BL31: Built : 13:46:23, Feb 27 2023
I/TC: 
I/TC: OP-TEE version: 3.20.0 (gcc version 9.2.1 20191025 (GNU Toolchain for the A-profile Architecture 9.2-2019.12 (arm-9.10))) #1 Mon Feb 27 13:47:09 UTC 2023 aarch64
I/TC: WARNING: This OP-TEE configuration might be insecure!
I/TC: WARNING: Please check https://urldefense.com/v3/__https://optee.readthedocs.io/en/latest/architecture/porting_guidelines.html__;!!G3vK!T_nXSXtu-qvW_vkh964FzhwwB5AjJLhRXzvpPgiyGv2gcrjLqxSETIl9Ls2rmGAMY9DIaQhV7zdYfhim6A$ 
I/TC: Primary CPU initializing
I/TC: SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
I/TC: HUK Initialized
I/TC: Activated SA2UL device
I/TC: Enabled firewalls for SA2UL TRNG device
I/TC: SA2UL TRNG initialized
I/TC: SA2UL Drivers initialized
I/TC: Primary CPU switching to normal world boot

U-Boot SPL 2021.01-00001-g1babd0e42c-dirty (Jan 17 2024 - 09:45:46 +0800)
EEPROM not available at 80, trying to read at 81
Reading on-board EEPROM at 0x51 failed 1
SYSFW ABI: 3.1 (firmware rev 0x0008 '8.6.4--v08.06.04 (Chill Capybar')
SPL malloc() before relocation used 0x2480 bytes (9 KB)
>>SPL: board_init_r()
spl_init
Trying to boot from MMC1
Authentication passed
Authentication passed
Jumping to U-Boot
loaded - jumping to U-Boot...
image entry point: 0x80800000


U-Boot 2023.04-dirty (Jan 18 2024 - 11:03:15 +0800)

SoC:   AM64X SR2.0 HS-FS
Model: Texas Instruments AM642 EVM
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
DRAM:  1 GiB
Core:  61 devices, 29 uclasses, devicetree: separate
NAND:  0 MiB
MMC:   mmc@fa10000: 0, mmc@fa00000: 1
Loading Environment from nowhere... OK
In:    serial@2800000
Out:   serial@2800000
Err:   serial@2800000
EEPROM not available at 0x50, trying to read at 0x51
Reading on-board EEPROM at 0x51 failed -121
Net:   eth0: ethernet@8000000port@1
Hit any key to stop autoboot:  0 
switch to partitions #0, OK
mmc0(part 0) is current device
SD/MMC found on device 0
Failed to load 'boot.scr'
Can't set block device
## Error: "main_cpsw0_qsgmii_phyinit" not defined
18493952 bytes read in 129 ms (136.7 MiB/s)
60741 bytes read in 27 ms (2.1 MiB/s)
Working FDT set to 88000000
## Flattened Device Tree blob at 88000000
   Booting using the fdt blob at 0x88000000
Working FDT set to 88000000
   Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
Working FDT set to 8feee000

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
[    0.000000] Linux version 6.1.46-rt13-gb871cdee8c31-dirty (cotrust@SZ) (aarch64-none-linux-gnu-gcc (Arm GNU Toolchain 11.3.Rel1) 11.3.1 20220712, GNU ld (Arm GNU Toolchain 11.3.Rel1) 2.38.20220708) #5 SMP PREEMPT_RT Thu Jan 18 15:43:28 CST 2024
[    0.000000] Machine model: Texas Instruments AM642 EVM
[    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
[    0.000000] printk: bootconsole [ns16550a0] enabled
[    0.000000] efi: UEFI not found.
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a0000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a0100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a0100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a1000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a1100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a2000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a2100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a2100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node r5f-dma-memory@a3000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a3100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node r5f-memory@a3100000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4000000, size 1 MiB
[    0.000000] OF: reserved mem: initialized node m4f-dma-memory@a4000000, compatible id shared-dma-pool
[    0.000000] Reserved memory: created DMA memory pool at 0x00000000a4100000, size 15 MiB
[    0.000000] OF: reserved mem: initialized node m4f-memory@a4100000, compatible id shared-dma-pool
[    0.000000] Zone ranges:
[    0.000000]   DMA      [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000]   DMA32    empty
[    0.000000]   Normal   empty
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000080000000-0x000000009e7fffff]
[    0.000000]   node   0: [mem 0x000000009e800000-0x00000000a57fffff]
[    0.000000]   node   0: [mem 0x00000000a5800000-0x00000000bfffffff]
[    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000000bfffffff]
[    0.000000] cma: Reserved 32 MiB at 0x00000000bcc00000
[    0.000000] psci: probing for conduit method from DT.
[    0.000000] psci: PSCIv1.1 detected in firmware.
[    0.000000] psci: Using standard PSCI v0.2 function IDs
[    0.000000] psci: Trusted OS migration not required
[    0.000000] psci: SMC Calling Convention v1.2
[    0.000000] percpu: Embedded 19 pages/cpu s39552 r8192 d30080 u77824
[    0.000000] Detected VIPT I-cache on CPU0
[    0.000000] CPU features: detected: GIC system register CPU interface
[    0.000000] CPU features: detected: ARM erratum 845719
[    0.000000] alternatives: applying boot alternatives
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 258048
[    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 omap2-nand.0:2m(NAND.tiboot3),2m(NAND.tispl),2m(NAND.tiboot3.backup),4m(NAND.u-boot),256k(NAND.u-boot-env),256k(NAND.u-boot-env.backup),-(NAND.file-system) root=PARTUUID=1723144d-01 rw rootfstype=ext4 rootwait
[    0.000000] Dentry cache hash table entries: 131072 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 65536 (order: 7, 524288 bytes, linear)
[    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
[    0.000000] Memory: 862320K/1048576K available (11136K kernel code, 1228K rwdata, 3620K rodata, 1920K init, 443K bss, 153488K reserved, 32768K cma-reserved)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu:     RCU event tracing is enabled.
[    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=2.
[    0.000000] rcu:     RCU priority boosting: priority 1 delay 500 ms.
[    0.000000] rcu:     RCU_SOFTIRQ processing moved to rcuc kthreads.
[    0.000000]  No expedited grace period (rcu_normal_after_boot).
[    0.000000]  Trampoline variant of Tasks RCU enabled.
[    0.000000]  Tracing variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
[    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=2
[    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
[    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
[    0.000000] GICv3: 256 SPIs implemented
[    0.000000] GICv3: 0 Extended SPIs implemented
[    0.000000] Root IRQ handler: gic_handle_irq
[    0.000000] GICv3: GICv3 features: 16 PPIs
[    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001840000
[    0.000000] ITS [mem 0x01820000-0x0182ffff]
[    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
[    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
[    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @80800000 (flat, esz 8, psz 64K, shr 0)
[    0.000000] ITS: using cache flushing for cmd queue
[    0.000000] GICv3: using LPI property table @0x0000000080030000
[    0.000000] GIC: using cache flushing for LPI property table
[    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000080040000
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
[    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
[    0.000001] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
[    0.000403] Console: colour dummy device 80x25
[    0.550388] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
[    0.550401] pid_max: default: 32768 minimum: 301
[    0.550483] LSM: Security Framework initializing
[    0.550647] Mount-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.550665] Mountpoint-cache hash table entries: 2048 (order: 2, 16384 bytes, linear)
[    0.553051] cblist_init_generic: Setting adjustable number of callback queues.
[    0.596087] cblist_init_generic: Setting shift to 1 and lim to 1.
[    0.602403] cblist_init_generic: Setting adjustable number of callback queues.
[    0.609790] cblist_init_generic: Setting shift to 1 and lim to 1.
[    0.616462] rcu: Hierarchical SRCU implementation.
[    0.616466] rcu:     Max phase no-delay instances is 1000.
[    0.616581] printk: bootconsole [ns16550a0] printing thread started
[    0.633750] Platform MSI: msi-controller@1820000 domain created
[    0.634302] EFI services will not be available.
[    0.634705] smp: Bringing up secondary CPUs ...
I/TC: Secondary CPU 1 initializing
I/TC: Secondary CPU 1 switching to normal world boot
[    0.659460] Detected VIPT I-cache on CPU1
[    0.659620] GICv3: CPU1: found redistributor 1 region 0:0x0000000001860000
[    0.659639] GICv3: CPU1: using allocated LPI pending table @0x0000000080050000
[    0.659701] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
[    0.659863] smp: Brought up 1 node, 2 CPUs
[    0.659871] SMP: Total of 2 processors activated.
[    0.659881] CPU features: detected: 32-bit EL0 Support
[    0.659887] CPU features: detected: CRC32 instructions
[    0.659961] CPU: All CPU(s) started at EL2
[    0.659964] alternatives: applying system-wide alternatives
[    0.661751] devtmpfs: initialized
[    0.676101] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
[    0.676130] futex hash table entries: 512 (order: 3, 32768 bytes, linear)
[    0.677782] pinctrl core: initialized pinctrl subsystem
[    0.678605] DMI not present or invalid.
[    0.679406] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.702383] DMA: preallocated 128 KiB GFP_KERNEL pool for atomic allocations
[    0.702562] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
[    0.702699] DMA: preallocated 128 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
[    0.702886] audit: initializing netlink subsys (disabled)
[    0.703936] thermal_sys: Registered thermal governor 'step_wise'
[    0.703948] thermal_sys: Registered thermal governor 'power_allocator'
[    0.704042] cpuidle: using governor menu
[    0.704304] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
[    0.704348] audit: type=2000 audit(0.700:1): state=initialized audit_enabled=0 res=1
[    0.741102] ASID allocator initialised with 65536 entries
[    0.758153] KASLR disabled due to lack of seed
[    0.768447] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
[    0.768463] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
[    0.768469] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
[    0.768473] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
[    0.768478] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
[    0.768482] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
[    0.768487] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
[    0.768490] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
[    0.770416] k3-chipinfo 43000014.chipid: Family:AM64X rev:SR2.0 JTAGID[0x1bb3802f] Detected
[    0.773415] iommu: Default domain type: Translated 
[    0.773430] iommu: DMA domain TLB invalidation policy: strict mode 
[    0.773912] SCSI subsystem initialized
[    0.774513] usbcore: registered new interface driver usbfs
[    0.774566] usbcore: registered new interface driver hub
a    0.774617] usbcore:I/ TrCeg:i sRteesreerdv edn esw hadreevidc eme mdroirvye irs  usebn
 bl[e d  
re.7I7/T5C23: 4]D ypnpams_icco rshe:a rLeidn umexPmoPSr y APiIs  veenrab.l 1e d
N giIs/teTrCe: d
 or[m  a l  W0.or77l5d2 3vi9r] tpuapls_iczoartei:on S osfuptwpaorrte  vies rd. i5sa.3b.l6e d-
lCoI/pyTrC:ig Ahts y2n0c0h5r-on2o0u07s  nRootdoilfifoc aGtiioomnes tatrie < gdiiosambetletid@
 inux.it>
[    0.775258] PTP clock support registered
[    0.775430] EDAC MC: Ver: 3.0.0
[    0.777113] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fc9100
[    0.777481] omap-mailbox 29040000.mailbox: omap mailbox rev 0x66fc9100
[    0.777705] omap-mailbox 29060000.mailbox: omap mailbox rev 0x66fc9100
[    0.778470] FPGA manager framework
[    0.780023] clocksource: Switched to clocksource arch_sys_counter
[    0.780605] VFS: Disk quotas dquot_6.6.0
[    0.780667] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
[    0.789603] NET: Registered PF_INET protocol family
[    0.789859] IP idents hash table entries: 16384 (order: 5, 131072 bytes, linear)
[    0.791687] tcp_listen_portaddr_hash hash table entries: 512 (order: 2, 20480 bytes, linear)
[    0.791731] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.791748] TCP established hash table entries: 8192 (order: 4, 65536 bytes, linear)
[    0.791883] TCP bind hash table entries: 8192 (order: 7, 655360 bytes, linear)
[    0.792737] TCP: Hash tables configured (established 8192 bind 8192)
[    0.793001] UDP hash table entries: 512 (order: 3, 49152 bytes, linear)
[    0.793105] UDP-Lite hash table entries: 512 (order: 3, 49152 bytes, linear)
[    0.793451] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.794459] RPC: Registered named UNIX socket transport module.
[    0.794470] RPC: Registered udp transport module.
[    0.794473] RPC: Registered tcp transport module.
[    0.794477] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.794489] NET: Registered PF_XDP protocol family
[    0.804080] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
[ itialise system trusted keyrings
[    1.113389] printk: console [    0.806644] workingset: timestamp_bits=46 max_order=18 bucket_order=0
[    0.815458] squashfs: version 4.0 (2009/01/31) Phillip Lo[ttyS2] printing thread started
ugher
[    1.113423] printk: console [ttyS2] enabled
[    1.113429] printk: bootconsole [ns16550a0] disabled
[    1.131587] printk: bootconsole [ns16550a0] printing thread stopped
[    1.134111] 2860000.serial: ttyS8 at MMIO 0x2860000 (irq = 321, base_baud = 3000000) is a 8250
[    1.139892] davinci_mdio 8000f00.mdio: Configuring MDIO in manual mode
[    1.180039] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
[    1.182442] davinci_mdio 8000f00.mdio: phy[1]: device 8000f00.mdio:01, driver unknown
[    1.182462] davinci_mdio 8000f00.mdio: phy[2]: device 8000f00.mdio:02, driver unknown
[    1.182545] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA00903, cpsw version 0x6BA80903 Ports: 3 quirks:00000006
[    1.182946] am65-cpsw-nuss 8000000.ethernet: Use random MAC address
[    1.182961] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.4
[    1.182968] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
[    1.183920] pps pps0: new PPS source ptp0
[    1.188477] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
[    1.207668] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 16
[    1.213381] am65-cpts 39000000.cpts: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:0
[    1.217826] mmc0: CQHCI version 5.10
[    1.221631] mmc1: CQHCI version 5.10
[    1.235586] 2810000.serial: ttyS3 at MMIO 0x2810000 (irq = 517, base_baud = 3000000) is a 8250
[    1.237597] 2820000.serial: ttyS4 at MMIO 0x2820000 (irq = 518, base_baud = 3000000) is a 8250
[    1.239364] 2830000.serial: ttyS5 at MMIO 0x2830000 (irq = 519, base_baud = 3000000) is a 8250
[    1.241247] 2850000.serial: ttyS7 at MMIO 0x2850000 (irq = 520, base_baud = 3000000) is a 8250
[    1.249254] debugfs: Directory 'pd:114' with parent 'pm_genpd' already present!
[    1.259026] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
[    1.345682] mmc0: Command Queue Engine enabled
[    1.345710] mmc0: new high speed MMC card at address 0001
[    1.346822] mmcblk0: mmc0:0001 88A19C 57.6 GiB 
[    1.362546]  mmcblk0: p1
[    1.363452] mmcblk0boot0: mmc0:0001 88A19C 4.00 MiB 
[    1.365253] mmcblk0boot1: mmc0:0001 88A19C 4.00 MiB 
[    1.366753] mmcblk0rpmb: mmc0:0001 88A19C 4.00 MiB, chardev (241:0)
[    2.741540] sdhci-am654 fa00000.mmc: Power on failed
[    2.772204] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
[    2.807550] EXT4-fs (mmcblk0p1): recovery complete
[    2.807924] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none.
[    2.812091] VFS: Mounted root (ext4 filesystem) on device 179:1.
[    2.813230] devtmpfs: mounted
[    2.814789] Freeing unused kernel memory: 1920K
[    2.814915] Run /sbin/init as init process
[    3.034618] systemd[1]: System time before build time, advancing clock.
[    3.071914] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
[    3.073096] systemd[1]: Detected architecture arm64.

Welcome to Arago 2023.10!

[    3.157372] systemd[1]: Hostname set to <am64xx-evm>.
[    3.320310] systemd-sysv-generator[151]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
[    3.601811] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[    3.601862] systemd[1]: Binding to IPv6 address not available since kernel does not support IPv6.
[    3.702225] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
[    3.789063] systemd[1]: Queued start job for default target Multi-User System.
[  OK  ] Created slice Slice /system/getty    3.886037] systemd[1]: Created slice Slice /system/getty.
0m.
[  OK  ] Created slice Slice /system/modprob[    3.914411] systemd[1]: Created slice Slice /system/modprobe.
e.
[  OK  ] Created slice Slice /system/serial-[    3.940783] systemd[1]: Created slice Slice /system/serial-getty.
getty.
[    3.967831] systemd[1]: Created slice User and Session Slice.
[  OK  ] Created slice User and Session Slice.
[  OK  ] Started Dispatch Password …ts to [    3.988868] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
Console Directory Watch.
[  OK  ] Started Forward Password R…uests [    4.012823] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
to Wall Directory Watch.
[  OK  ] Reached target Path Units.[    4.036732] systemd[1]: Reached target Path Units.

[  OK  ] Reached target Remote File Systems   4.056406] systemd[1]: Reached target Remote File Systems.
[0m.
[  OK  ] Reached target Slice Units.[    4.076406] systemd[1]: Reached target Slice Units.

[  OK  ] Reached target Swaps.
[    4.096441] systemd[1]: Reached target Swaps.
[  OK  ] Listening on RPCbind Server Activat[    4.141462] systemd[1]: Listening on RPCbind Server Activation Socket.
ion Socket.
[  OK  ] Reached target RPC Port Mapper.[    4.164544] systemd[1]: Reached target RPC Port Mapper.

[  OK  ] Listening on Process Core Dump Sock[    4.193101] systemd[1]: Listening on Process Core Dump Socket.
et.
[  OK  ] Listening on initctl Compatibility [    4.216934] systemd[1]: Listening on initctl Compatibility Named Pipe.
Named Pipe.
[  OK  ] Listening on Journal Audit Socket    4.241607] systemd[1]: Listening on Journal Audit Socket.
0m.
[  OK  ] Listening on Journal Socket (/dev/l[    4.265345] systemd[1]: Listening on Journal Socket (/dev/log).
og).
[  OK  ] Listening on Journal Socket.
[    4.289411] systemd[1]: Listening on Journal Socket.
[  OK  ] Listening on Network Service Netlin[    4.301833] systemd[1]: Listening on Network Service Netlink Socket.
k Socket.
[  OK  ] Listening on udev Control Socket    4.325585] systemd[1]: Listening on udev Control Socket.
m.
[  OK  ] Listening on udev Kernel Socket[    4.349221] systemd[1]: Listening on udev Kernel Socket.
.
[  OK  ] Listening on User Database Manager [    4.375495] systemd[1]: Listening on User Database Manager Socket.
Socket.
         Mounting Huge Pages File System...[    4.425074] systemd[1]: Mounting Huge Pages File System...

         Mounting POSIX Message Queue File System..[    4.456308] systemd[1]: Mounting POSIX Message Queue File System...
.
         Mounting Kernel Debug File System...[    4.488446] systemd[1]: Mounting Kernel Debug File System...

[    4.508955] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
         Mounting Temporary Directory /tmp...[    4.533147] systemd[1]: Mounting Temporary Directory /tmp...

[    4.556751] systemd[1]: Create List of Static Device Nodes was skipped because of a failed condition check (ConditionFileNotEmpty=/lib/modules/6.1.46-rt13-gb871cdee8c31-dirty/modules.devname).
         Starting Load Kernel Module configfs...[    4.564515] systemd[1]: Starting Load Kernel Module configfs...

[    4.607722] systemd[1]: Starting Load Kernel Module drm...
         Starting Load Kernel Module drm...
         Starting Load Kernel Module fuse...[    4.661558] systemd[1]: Starting Load Kernel Module fuse...

         Starting RPC Bind...
[    4.695041] systemd[1]: Starting RPC Bind...
[    4.704683] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
         Starting Journal Service...[    4.718968] systemd[1]: Starting Journal Service...

         Starting Load Kernel Modules...[    4.769643] systemd[1]: Starting Load Kernel Modules...

         Starting Generate network …ts from Kernel co[    4.805200] systemd[1]: Starting Generate network units from Kernel command line...
mmand line...
         Starting Remount Root and Kernel File Systems   4.869188] systemd[1]: Starting Remount Root and Kernel File Systems...
[0m...
         Starting Coldplug All udev Devices...[    4.910111] systemd[1]: Starting Coldplug All udev Devices...

[  OK  ] Started RPC Bind.[    4.950712] systemd[1]: Started RPC Bind.

[  OK  ] Mounted Huge Pages File System.[    4.969633] systemd[1]: Mounted Huge Pages File System.

[  OK  ] Mounted POSIX Message Queue File Sy[    4.997310] systemd[1]: Mounted POSIX Message Queue File System.
stem.
[  OK  ] Mounted Kernel Debug File System    5.021456] systemd[1]: Mounted Kernel Debug File System.
m.
[    5.022523] EXT4-fs (mmcblk0p1): re-mounted. Quota mode: none.
[  OK  ] Mounted Temporary Directory /tmp    5.054627] systemd[1]: Mounted Temporary Directory /tmp.
m.
[  OK  ] Started Journal Service.[    5.081356] systemd[1]: Started Journal Service.

[  OK  ] Finished Load Kernel Module configfs.
[  OK  ] Finished Load Kernel Module drm.
[  OK  ] Finished Load Kernel Module fuse.
[FAILED] Failed to start Load Kernel Modules.
See 'systemctl status systemd-modules-load.service' for details.
[  OK  ] Finished Generate network units from Kernel command line.
[  OK  ] Finished Remount Root and Kernel File Systems.
         Mounting Kernel Configuration File System...
         Starting Flush Journal to Persistent Storage...
         Starting Apply Kernel Variables...
[    5.374164] systemd-journald[162]: Received client request to flush runtime journal.
         Starting Create Static Device Nodes in /dev...
[  OK  ] Mounted Kernel Configuration File System.
[  OK  ] Finished Flush Journal to Persistent Storage.
[  OK  ] Finished Apply Kernel Variables.
[  OK  ] Finished Create Static Device Nodes in /dev.
[  OK  ] Reached target Preparation for Local File Systems.
         Mounting /media/ram...
         Mounting /var/volatile...
[    5.588607] audit: type=1334 audit(1651167747.556:2): prog-id=5 op=LOAD
[    5.590042] audit: type=1334 audit(1651167747.556:3): prog-id=6 op=LOAD
         Starting Rule-based Manage…for Device Events and Files...
[  OK  ] Mounted /media/ram.
[  OK  ] Mounted /var/volatile.
         Starting Load/Save Random Seed...
[  OK  ] Reached target Local File Systems.
         Starting Create Volatile Files and Directories...
[  OK  ] Finished Create Volatile Files and Directories.
         Starting Network Time Synchronization...
         Starting Record System Boot/Shutdown in UTMP...
[  OK  ] Started Rule-based Manager for Device Events and Files.
[  OK  ] Finished Coldplug All udev Devices.
[  OK  ] Finished Record System Boot/Shutdown in UTMP.
[    6.784157] random: crng init done
[  OK  ] Finished Load/Save Random Seed.
[    6.823362] systemd-journald[162]: Oldest entry in /run/log/journal/5e4600aa5bce48f0b15c457528a74d67/system.journal is older than the configured file retention duration (1month), suggesting rotation.
[  OK  ] Started Network Time Synchronizatio[    6.823397] systemd-journald[162]: /run/log/journal/5e4600aa5bce48f0b15c457528a74d67/system.journal: Journal header limits reached or header out-of-date, rotating.
n.
[  OK  ] Reached target System Initialization.
[  OK  ] Started Daily Cleanup of Temporary Directories.
[  OK  ] Reached target System Time Set.
[  OK  ] Reached target Timer Units.
[  OK  ] Listening on Avahi mDNS/DNS-SD Stack Activation Socket.
[  OK  ] Listening on D-Bus System Message Bus Socket.
         Starting Docker Socket for the API...
[  OK  ] Listening on dropbear.socket.
         Starting D-Bus System Message Bus...
[  OK  ] Listening on Docker Socket for the API.
[  OK  ] Reached target Socket Units.
[  OK  ] Found device /dev/ttyS2.
[  OK  ] Started D-Bus System Message Bus.
[  OK  ] Reached target Basic System.
         Starting Print notice about GPLv3 packages...
         Starting IPv6 Packet Filtering Framework...
         Starting IPv4 Packet Filtering Framework...
         Starting Expand the rootfs…ll size of the boot device....
[    7.578547] audit: type=1334 audit(1705564605.426:4): prog-id=7 op=LOAD
         Starting User Login Management...[    7.579086] audit: type=1334 audit(1705564605.426:5): prog-id=8 op=LOAD

[  OK  ] Started TEE Supplicant.
         Starting Telnet Server...
[  OK  ] Finished IPv6 Packet Filtering Framework.
[  OK  ] Finished IPv4 Packet Filtering Framework.
[  OK  ] Reached target Preparation for Network.
         Starting Network Configuration...
[  OK  ] Finished Telnet Server.
[  OK  ] Finished Expand the rootfs…full size of the boot device..
[  OK  ] Started User Login Management.
[  OK  ] Started Network Configuration.
         Starting Network Name Resolution...
[    8.800808] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:02] driver [Generic PHY] (irq=POLL)
[    8.800844] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode
[    8.927403] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:01] driver [Generic PHY] (irq=POLL)
[    8.927439] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  OK  ] Started Network Name Resolution.
[  OK  ] Reached target Network.
[  OK  ] Reached target Host and Network Name Lookups.
         Starting Avahi mDNS/DNS-SD Stack...
         Starting containerd container runtime...
[  OK  ] Started Netperf Benchmark Server.
***************************************************************
***************************************************************
NOTICE: This file system contains the following GPL-3.0 packages:
        bash
        cifs-utils
        dosfstools
        grub-common
        grub-editenv
        grub-efi
        less
        libdw1
        libelf1
        libgcc1
        libreadline8
        libstdc++6
        parted

If you do not wish to distribute GPL-3.0 components please remove
the above packages prior to distribution.  This can be done using
the opkg remove command.  i.e.:
    opkg remove <package>
Where <package> is the name printed in the list above

NOTE: If the package is a dependency of another package you
      will be notified of the dependent packages.  You should
      use the --force-removal-of-dependent-packages option to
      also remove the dependent packages as well
***************************************************************
***************************************************************
[  OK  ] Started NFS status monitor for NFSv2/3 locking..
         Starting Permit User Sessions...
[  OK  ] Finished Print notice about GPLv3 packages.
[  OK  ] Started Avahi mDNS/DNS-SD Stack.
[  OK  ] Finished Permit User Sessions.
[  OK  ] Started Getty on tty1.
[  OK  ] Started Serial Getty on ttyS2.
[  OK  ] Reached target Login Prompts.
         Starting Synchronize System and HW clocks...
[FAILED] Failed to start Synchronize System and HW clocks.
See 'systemctl status sync-clocks.service' for details.
[   11.498666] icssg-prueth icssg0-eth: port 1: using random MAC addr: 1a:3d:06:46:99:d7
[   11.503515] icssg-prueth icssg0-eth: port 2: using random MAC addr: 1a:cc:d8:9d:0f:68
[   11.505368] Generic PHY 30032400.mdio:02: attached PHY driver (mii_bus:phy_addr=30032400.mdio:02, irq=POLL)
[   11.506626] Generic PHY 30032400.mdio:03: attached PHY driver (mii_bus:phy_addr=30032400.mdio:03, irq=POLL)
[   11.506653] icssg-prueth icssg0-eth: TI PRU ethernet driver initialized: dual EMAC mode
[   11.749330] remoteproc remoteproc0: powering up 30034000.pru
[   11.753798] remoteproc remoteproc0: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 40936
[   11.753843] remoteproc remoteproc0: unsupported resource 5
[   11.753873] remoteproc remoteproc0: remote processor 30034000.pru is now up
[   11.753931] remoteproc remoteproc1: powering up 30004000.rtu
[   11.755516] remoteproc remoteproc1: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30884
[   11.755572] remoteproc remoteproc1: remote processor 30004000.rtu is now up
[   11.755623] remoteproc remoteproc2: powering up 3000a000.txpru
[   11.761452] remoteproc remoteproc2: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 36672
[   11.761511] remoteproc remoteproc2: remote processor 3000a000.txpru is now up
[   11.761814] remoteproc remoteproc3: powering up 30038000.pru
[   11.763690] remoteproc remoteproc3: Booting fw image ti-pruss/am65x-sr2-pru1-prueth-fw.elf, size 41208
[   11.763732] remoteproc remoteproc3: unsupported resource 5
[   11.763762] remoteproc remoteproc3: remote processor 30038000.pru is now up
[   11.763817] remoteproc remoteproc4: powering up 30006000.rtu
[   11.772250] remoteproc remoteproc4: Booting fw image ti-pruss/am65x-sr2-rtu1-prueth-fw.elf, size 30124
[   11.772306] remoteproc remoteproc4: remote processor 30006000.rtu is now up
[   11.772364] remoteproc remoteproc5: powering up 3000c000.txpru
[   11.774638] remoteproc remoteproc5: Booting fw image ti-pruss/am65x-sr2-txpru1-prueth-fw.elf, size 35184
[   11.774707] remoteproc remoteproc5: remote processor 3000c000.txpru is now up
[   11.780821] pps pps1: new PPS source ptp2
[  OK  ] Started containerd container runtime.
[  OK  ] Reached target Multi-User System.
         Starting Record Runlevel Change in UTMP...
[  OK  ] Finished Record Runlevel Change in UTMP.

 _____                    _____           _         _   
|  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
|     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
|__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
              |___|                    |___|            

Arago Project am64xx-evm -

Arago 2023.10 am64xx-evm -

am64xx-evm login: [   13.952358] icssg-prueth icssg0-eth eth2: Link is Up - 100Mbps/Full - flow control off
root
[  112.608199] audit: type=1334 audit(1705564710.454:6): prog-id=9 op=LOAD
[  112.609172] audit: type=1334 audit(1705564710.458:7): prog-id=10 op=LOAD
[  113.186502] audit: type=1006 audit(1705564711.034:8): pid=449 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=1 res=1
[  113.186537] audit: type=1300 audit(1705564711.034:8): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=ffffe5e2f7c8 a2=1 a3=ffffa1557020 items=0 ppid=1 pid=449 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
[  113.186553] audit: type=1327 audit(1705564711.034:8): proctitle="(systemd)"
[  113.262175] audit: type=1334 audit(1705564711.110:9): prog-id=11 op=LOAD
[  113.262330] audit: type=1300 audit(1705564711.110:9): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=ffffe48792f0 a2=78 a3=0 items=0 ppid=1 pid=449 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="systemd" exe="/lib/systemd/systemd" key=(null)
[  113.262384] audit: type=1327 audit(1705564711.110:9): proctitle="(systemd)"
[  113.262511] audit: type=1334 audit(1705564711.110:10): prog-id=11 op=UNLOAD
[  113.262959] audit: type=1334 audit(1705564711.110:11): prog-id=12 op=LOAD
root@am64xx-evm:~# 
root@am64xx-evm:~# ifconfig 
eth0      Link encap:Ethernet  HWaddr 34:08:E1:84:AD:1B  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth1      Link encap:Ethernet  HWaddr EE:01:02:1B:91:28  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

eth2      Link encap:Ethernet  HWaddr FA:10:E8:1E:8C:12  
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:6 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:2004 (1.9 KiB)

eth3      Link encap:Ethernet  HWaddr E6:3B:01:DD:E5:0C  
          UP BROADCAST MULTICAST  MTU:1500  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

lo        Link encap:Local Loopback  
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:65536  Metric:1
          RX packets:90 errors:0 dropped:0 overruns:0 frame:0
          TX packets:90 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000 
          RX bytes:6824 (6.6 KiB)  TX bytes:6824 (6.6 KiB)

root@am64xx-evm:~# 

  • Hello Tony,

    I am running tests on TMDS64EVM (AM64x HS-FS silicon), with the lower port on the two-port stack. I can observe a similar output as this other customer here: 
    https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1294983/am6442-icssg-ethernet-driver-crash-intermittent-similar-to-1158425 

    (where this test was run on Linux SDK 9.0)

    [   24.688781] TI DP83869 300b2400.mdio:0f: selected op-mode is not valid with MII mode
    [   24.697909] icssg-prueth icssg1-eth: couldn't connect to phy ethernet-phy@0
    [   24.708623] Unable to handle kernel NULL pointer dereference at virtual address 0000000000000358
    [   24.718102] Mem abort info:
    [   24.721572]   ESR = 0x0000000096000006
    [   24.725931]   EC = 0x25: DABT (current EL), IL = 32 bits
    [   24.733594]   SET = 0, FnV = 0
    [   24.737283]   EA = 0, S1PTW = 0
    [   24.741095]   FSC = 0x06: level 2 translation fault
    [   24.746661] Data abort info:
    [   24.749566]   ISV = 0, ISS = 0x00000006
    [   24.754254]   CM = 0, WnR = 0
    [   24.757696] user pgtable: 4k pages, 48-bit VAs, pgdp=000000008381e000
    [   24.764703] [0000000000000358] pgd=080000008384b003, p4d=080000008384b003, pud=080000008394c003, pmd=0000000000000000
    [   24.775874] Internal error: Oops: 0000000096000006 [#1] PREEMPT SMP
    [   24.782166] Modules linked in: pci_endpoint_test rpmsg_ctrl rpmsg_char cdns3 cdns_usb_common irq_pruss_intc overlay icssg_prueth crct10dif_ce pru_rproc icss_iep hsr phy_c
    an_transceiver ti_k3_m4_remoteproc ti_k3_common pci_j721e_host pci_j721e pcie_cadence_host cdns3_ti pcie_cadence wlcore_sdio wl18xx ti_k3_r5_remoteproc wlcore virtio_rpmsg_b
    us mac80211 libarc4 rpmsg_ns cfg80211 rfkill m_can_platform pwm_tiecap m_can sa2ul can_dev spi_omap2_mcspi pruss optee_rng rng_core cryptodev(O) fuse drm drm_panel_orientati
    on_quirks ipv6
    [   24.828739] CPU: 1 PID: 99 Comm: kworker/u4:2 Tainted: G           O       6.1.33-g40c32565ca #1
    [   24.837522] Hardware name: Texas Instruments AM642 EVM (DT)
    [   24.843089] Workqueue: events_unbound deferred_probe_work_func
    [   24.848944] pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
    [   24.855900] pc : phy_attached_print+0x28/0x1b0
    [   24.860355] lr : phy_attached_info+0x14/0x20
    [   24.864629] sp : ffff8000097eba20
    [   24.867938] x29: ffff8000097eba20 x28: ffff0000067b2940 x27: ffff0000040d24c0
    [   24.875070] x26: ffff0000040d2508 x25: 0000000000040000 x24: ffff0000003fe400
    [   24.882200] x23: ffff0000003fe410 x22: ffff00007fc2bbf0 x21: 0000000000000000
    [   24.889328] x20: 0000000000000000 x19: 0000000000000000 x18: 0000000000000000
    [   24.896455] x17: 0000000000000000 x16: 0000000000000000 x15: 00004650ca137854
    [   24.903583] x14: 000000000000002a x13: 000000000000002a x12: 0000000000000000
    [   24.910711] x11: 0000000000000004 x10: 00000000000009b0 x9 : ffff8000097eb7c0
    [   24.917837] x8 : ffff0000012b8000 x7 : ffff00007fbd3340 x6 : 0000000000000000
    [   24.924964] x5 : ffff00007fbccb60 x4 : ffff00007fbccb60 x3 : 0000000000000000
    [   24.932092] x2 : 0000000000000000 x1 : 0000000000000000 x0 : 0000000000000000
    [   24.939221] Call trace:
    [   24.941658]  phy_attached_print+0x28/0x1b0
    [   24.945755]  phy_attached_info+0x14/0x20
    [   24.949674]  prueth_probe+0x478/0x960 [icssg_prueth]
    [   24.954655]  platform_probe+0x68/0xe0
    [   24.958313]  really_probe+0xbc/0x2dc
    [   24.961885]  __driver_probe_device+0x78/0x114
    [   24.966237]  driver_probe_device+0xd8/0x15c
    [   24.970414]  __device_attach_driver+0xb8/0x134
    [   24.974848]  bus_for_each_drv+0x78/0xd0
    [   24.978679]  __device_attach+0xa8/0x1c0
    [   24.982510]  device_initial_probe+0x14/0x20
    [   24.986685]  bus_probe_device+0x9c/0xa4
    [   24.990515]  deferred_probe_work_func+0x88/0xc0
    [   24.995039]  process_one_work+0x1d0/0x320
    [   24.999043]  worker_thread+0x2c8/0x444
    [   25.002784]  kthread+0x10c/0x110
    [   25.006009]  ret_from_fork+0x10/0x20
    [   25.009585] Code: a9025bf5 aa0103f5 a9080fe2 f9004be4 (f941ac02)
    [   25.015666] ---[ end trace 0000000000000000 ]---
    [   25.029005] remoteproc remoteproc13: powering up 300b4000.pru
    [   25.041143] remoteproc remoteproc13: Booting fw image ti-pruss/am65x-sr2-pru0-prueth-fw.elf, size 38800
    [   25.050702] remoteproc remoteproc13: unsupported resource 5
    [   25.056328] remoteproc remoteproc13: remote processor 300b4000.pru is now up
    [   25.063463] remoteproc remoteproc14: powering up 30084000.rtu
    [   25.073415] remoteproc remoteproc14: Booting fw image ti-pruss/am65x-sr2-rtu0-prueth-fw.elf, size 30968
    [   25.082898] remoteproc remoteproc14: remote processor 30084000.rtu is now up
    [   25.089997] remoteproc remoteproc7: powering up 3008a000.txpru
    [   25.099952] remoteproc remoteproc7: Booting fw image ti-pruss/am65x-sr2-txpru0-prueth-fw.elf, size 37328
    [   25.109520] remoteproc remoteproc7: remote processor 3008a000.txpru is now up
    [   25.118020] Unable to handle kernel NULL pointer dereference at virtual address 00000000000004e8
    [   25.126883] Mem abort info:
    [   25.129682]   ESR = 0x0000000096000006
    [   25.133437]   EC = 0x25: DABT (current EL), IL = 32 bits
    [   25.138770]   SET = 0, FnV = 0
    [   25.141820]   EA = 0, S1PTW = 0
    [   25.144963]   FSC = 0x06: level 2 translation fault
    [   25.149847] Data abort info:
    [   25.152738]   ISV = 0, ISS = 0x00000006
    [   25.156578]   CM = 0, WnR = 0
    [   25.159566] user pgtable: 4k pages, 48-bit VAs, pgdp=00000000866df000
    [   25.166014] [00000000000004e8] pgd=0800000086687003, p4d=0800000086687003, pud=0800000086504003, pmd=0000000000000000
    [   25.176642] Internal error: Oops: 0000000096000006 [#2] PREEMPT SMP
    [   25.182905] Modules linked in: pci_endpoint_test rpmsg_ctrl rpmsg_char cdns3 cdns_usb_common irq_pruss_intc overlay icssg_prueth crct10dif_ce pru_rproc icss_iep hsr phy_c
    an_transceiver ti_k3_m4_remoteproc ti_k3_common pci_j721e_host pci_j721e pcie_cadence_host cdns3_ti pcie_cadence wlcore_sdio wl18xx ti_k3_r5_remoteproc wlcore virtio_rpmsg_b
    us mac80211 libarc4 rpmsg_ns cfg80211 rfkill m_can_platform pwm_tiecap m_can sa2ul can_dev spi_omap2_mcspi pruss optee_rng rng_core cryptodev(O) fuse drm drm_panel_orientati
    on_quirks ipv6
    [   25.229454] CPU: 1 PID: 225 Comm: systemd-network Tainted: G      D    O       6.1.33-g40c32565ca #1
    [   25.238572] Hardware name: Texas Instruments AM642 EVM (DT)
    [   25.244132] pstate: 80000005 (Nzcv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
    [   25.251080] pc : mutex_lock+0x2c/0x6c
    [   25.254749] lr : phy_start+0x20/0xbc
    [   25.258321] sp : ffff800009eb3480
    [   25.261625] x29: ffff800009eb3480 x28: ffff800009eb3530 x27: 0000000000000001
    [   25.268754] x26: 0000000000000001 x25: ffff0000067b0ed8 x24: ffff0000067b1480
    [   25.275882] x23: ffff0000040d2480 x22: 0000000000000220 x21: 00000000000001e8
    [   25.283009] x20: 00000000000004e8 x19: 0000000000000000 x18: ffffffffffffffff
    [   25.290137] x17: 7520776f6e207369 x16: 2075727078742e30 x15: 000000000000006a
    [   25.297265] x14: 0000000000000375 x13: 0000000000000001 x12: 0000000000000000
    [   25.304391] x11: 0000000000000001 x10: 00000000000009b0 x9 : ffff800009eb32a0
    [   25.311519] x8 : ffff00007fbcd180 x7 : 0800000000002000 x6 : 0000000c875b8f28
    [   25.318647] x5 : 03ffffffffffffff x4 : 0000000000000000 x3 : 00000000000004e8
    [   25.325773] x2 : ffff000000d6c740 x1 : 0000000000000000 x0 : 00000000000004e8
    [   25.332902] Call trace:
    [   25.335340]  mutex_lock+0x2c/0x6c
    [   25.338652]  emac_ndo_open+0x7d4/0xb3c [icssg_prueth]
    [   25.343716]  __dev_open+0xec/0x1dc
    [   25.347117]  __dev_change_flags+0x190/0x20c
    [   25.351293]  dev_change_flags+0x24/0x64
    [   25.355124]  do_setlink+0x234/0xe4c
    [   25.358609]  rtnl_setlink+0xe0/0x180
    [   25.362178]  rtnetlink_rcv_msg+0x12c/0x390
    [   25.366267]  netlink_rcv_skb+0x5c/0x130
    [   25.370097]  rtnetlink_rcv+0x18/0x24
    [   25.373666]  netlink_unicast+0x2d8/0x330
    [   25.377579]  netlink_sendmsg+0x1ac/0x410
    [   25.381493]  __sys_sendto+0x128/0x164
    [   25.385147]  __arm64_sys_sendto+0x28/0x3c
    [   25.389147]  invoke_syscall+0x48/0x114
    [   25.392893]  el0_svc_common.constprop.0+0xd4/0xfc
    [   25.397591]  do_el0_svc+0x30/0xd0
    [   25.400900]  el0_svc+0x2c/0x84
    [   25.403951]  el0t_64_sync_handler+0xbc/0x140
    [   25.408212]  el0t_64_sync+0x18c/0x190
    [   25.411873] Code: b5000140 d65f03c0 d2800001 f9800071 (c85ffc60)
    [   25.417953] ---[ end trace 0000000000000000 ]---
    
    am64xx-evm login: root
    

    Do the patches suggested in that other thread help the customer?

    I am double-checking with the developer on his current status of debugging the issue on the ti-linux-kernel.

    Regards,

    Nick

  • Hello Tony,

    The developer is going to try to address this for SDK 9.2, but he does not have any major updates for us at this point in time.

    Regards,

    Nick

  • Time flies,

    customer checked on SDK9.2, the PRU MII still doesn't work.

  • Hello Tony,

    Thanks for bringing this back up. Which SDK 9.2 release did they test? (9.2.0, 9.2.1.9, or 9.2.1.10)

    SDK 10.0 just released today. I have not heard anything from the developer since our last communication, so I'm not sure if they did any additional work to fix this on the ti-linux-kernel branch for SDK 10.0 or not. I'll check in with them.

    Regards,

    Nick

  • Heads-up, today is a holiday in India, and the developer might be on vacation for the rest of the week. Feel free to ping the thread if we haven't responded by Monday.

    Regards,

    Nick

  • #1. Customer said he tested with all 3 SDK9.2.x version, either work.

    #2. I see in release notes, 9.2.1.9, or 9.2.1.10, both have LCPD-37223 resolved item, which version resolved this issue? or not actually。

    #3. SDK 10.x did not mention LCPD-37223. customer will double check with 9.2.1.10 again.

  • For future readers, we're still working on getting clarity from the developer in the background on exactly what is expected to be working on which SDK releases.

    Regards,

    Nick

  • Hello Tony,

    Checking in. Is MII mode still not working for the customer?

    Regards,

    Nick

  • Hello Nick,

    I would like to ask if SDK8.6 supports the MII method for ICSSG?At present, I have not enabled the Ethernet in MII mode on 8.6.

  • As my first post, ICSSG MII mode works on SDK8.6. my customer verified it.

  • Hi,

    I saw what you mentioned before and compared it with your customer devicetree.that is, the kernel is fully supported.Which PHY are you using?I use DP83620 ,but I just haven’t tuned it in yet.Can I send our devicetree?Can you help analyze it?Thank you very much!

  • Hello,

    Can I ask if you are using SDK8.06.00.42? Or is it another version?

  • Hi,

    Closing this thread, as there is no response for long. Feel free to ping, if you want to continue discussion.

    Regards

    Ashwani

  • ICSSG MII works on SDK10.0