This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDX654IDKEVM: Dev board often not booting on power on, Needing PoR button to be pressed

Part Number: TMDX654IDKEVM

When powering on TMDX654IDEVM kit roughly 1/2 time receive no console output on the debug UART,
This can be recovered by the POR switch (SW8),

We have two eval boards - It only occurs on 1 of the two

I've checked some of the voltage tp's such as the input voltages, output 12V's and some of the rails. As well as comparing them to the other eval board,

We have not changed any of the jumper / boot switch settings on either of the units, They are both setup to boot from SD card in the MMC slot,
There is no output when it occurs through so it does not look like it has got that far.

We are using the SDI65-24-UD-P6 which is one of the example plug packs in the quick start guide, 
We don't have anything added via PCIE or added on boards such as the LCD kit.
We do have the ethernet ports used.

We are not using the TI development image, However the behavior is the same when I change the SD card image to a TI development kit image,


I would like to get this board booting cleanly after being powered,
Is there any different information I should provide,
Particular signals I should be checking.