This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: Kernel crash due to clean dma

Part Number: TDA4VH-Q1
Other Parts Discussed in Thread: TDA4VH

SDK: RTOS_8.6

Board: TDA4VH evm

I found that a kernel crash problem occurs in the following two situations:

1. The same dma memory is input to v4l2 encoding and the appMemCacheW function is used to refresh this memory. When multiple threads run concurrently, the kernel will crash.,(Attached codelibmediacodectest.tar The testMediaCodec inside is a program that can reproduce the problem)

2.Using 2 colorconvert nodes to convert the same dma memory will cause the kernel to crash when running concurrently with multiple threads.

Below is the kernel crash log

Use the program I sent and it can be reproduced on the development board under SDK 8.6