Other Parts Discussed in Thread: OMAP3530, DM3730
Not being Linux expert, in using the OMAP3530 we would like to simplify the design by NOT using Linux. The design is really straightforward. The ARM processor has to handle the user interface and control the receiver functions. The DSP has to do the CODEC and also allow for future operational enhancements. We don't need Linux to run the ARM code, and I'm not sure we need it for any of the DSP stuff beside the CODEC (MPEG4 encode).
Could you provide suggestions / guidance on our options for this design? Would C6EZACCEL software be a good tool for this design? Is the MPEG4 encode part of the OpenCV + VLIB's, see attachment.
6014.OpenCV_on_TIs_DSP+ARM_spry175.pdf
-Tom-