This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem with debugging in c28x when using RTSC



When trying to run the following simple program:

main.cfg:

var System = xdc.useModule('xdc.runtime.System');
System.SupportProxy = xdc.useModule('xdc.runtime.SysStd');

main.c

#include <xdc/runtime/Types.h>
#include <xdc/runtime/System.h>

int main()
{
    System_printf("Hello world!\n");
    return 0;
}

using ccsv4 and a ezdsp28335, i cannot seem to get any output in the console. Furthermore, I need to use the clock (Target menu -> clock) to benchmark a slightly more complex code, but when I try to do it I get:

C28xx: Error programming AET Job: This task cannot be accomplished with the existing AET resources.

Needles to say, I am getting the same problems when using a sys/bios based program.

What does this mean? What can I do?

Thanks,

Sebastian