Part Number: AM6442
Other Parts Discussed in Thread: TMDS64EVM
When I run the ethercat_slave_simple_demo_am64x-evm_r5fss0-0_freertos_ti-arm-clan,the corresponding SDK version is ind_comms_sdk_am64x_09_00_00_03, the corresponding hardware circuit is TMDS64EVM, the program prints a prompt saying that the PHY could not be found

I modified the program to add a phyid on print, and it shows that the phyid of the input function is 0
Phy Reset: 1.35
Phy Reset: 0.17
Phy UnReset: 1.35
Phy UnReset: 0.17
Configure Phy bits: PhyAddr:5, LinPol:HIGH, PhyAddr:3, LinPol:LOW, (0x8)
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
phy_id:0
PRU_PHY_detect:156 PHY0 not ok
phy_id:0
PRU_PHY_detect:164 PHY1 not ok
No PHYs found !!!
PRU_MDIO_initPhy: 0x120003 EC is fatal=1, SRC:PRU_MDIO_initPhy:339