Part Number: TDA4VM
1. I run linux on TDA4, using the default ti-processor-sdk-linux-j7-evm-08_06_00_11/board-support/ build-images /tiboot3.bin, I read the documentation that this tiboot3 is r5 spl
2. I want to update tispl.bin via AB partition, in order to do this I need a level above tispl, which is the r5 spl operation flag bit, but I can't find the tiboot3 source code in linux
sdk is only pre-compiled, I want to change the tiboot3 code, I did not find this source code in the RTOS SDK, \packages\ti\boot\sbl path only SBL boot-related
3. Can you help me answer the following questions?