Hello,
I'm running video D1 capturing on DM365 under Linux (simple QBUF/DQBUF loop on v4l device, not through DMAI). The 'top' shows that the process takes about 0% of CPU load. But each 4.5 minutes CPU load of the process rises up to 25% for 3-5 seconds.
During test every possible non-related task or service are disabled.
When testing it on Kernels 2.6.18, 2.6.32, 2.6.37, we get the same results.
What can be the cause?
Thanks in advance.