This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SK-AM62A-LP: Ethernet doesn't establish a connection (using DHCP or a static IP) after using systemd config file to set a static IP address

Part Number: SK-AM62A-LP

I've been using using SDK9.0.0.8 the the SK-AM62A-LP rev E3 for months in DHCP mode. I then had a need to use a static IP address on wired connection eth0 instead of using DHCP. It seemed after a little searching that the proper way to do this was to edited the /etc/systemd/networking/10-eth.network file as such:

[Match]
Name=eth0
KernelCommandLine=!root=/dev/nfs

[Network]
# DHCP=yes
Address=10.60.23.55/23
Gateway=10.60.23.254

Upon rebooting and even power cycling a few times it was all working properly and connecting on a small isolated network. However after powering it on today, I am unable to communicate with it or see any communication. I don't rightly know of anything I could have done to cause this as it seems that no data is getting output from the AM62A-LP board ethernet cable while examining the network using Wireshark.

Here are some things I've tried recently from an SD card using a clean image of the provided SDK 9.0 (so it should be back to using DHCP like I was originally using):

root@am62axx-evm:/# ping 192.168.10.133
PING 192.168.10.133 (192.168.10.133): 56 data bytes
ping: sendto: Network is unreachable
root@am62axx-evm:/# ethtool eth0
Settings for eth0:
        Supported ports: [ TP    MII ]
        Supported link modes:   10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Full
        Supported pause frame use: Symmetric
        Supports auto-negotiation: Yes
        Supported FEC modes: Not reported
        Advertised link modes:  10baseT/Half 10baseT/Full
                                100baseT/Half 100baseT/Full
                                1000baseT/Full
        Advertised pause frame use: Symmetric
        Advertised auto-negotiation: Yes
        Advertised FEC modes: Not reported
        Link partner advertised link modes:  10baseT/Half 10baseT/Full
                                             100baseT/Half 100baseT/Full
                                             1000baseT/Full
        Link partner advertised pause frame use: Symmetric
        Link partner advertised auto-negotiation: Yes
        Link partner advertised FEC modes: Not reported
        Speed: 1000Mb/s
        Duplex: Full
        Auto-negotiation: on
        master-slave cfg: preferred slave
        master-slave status: slave
        Port: Twisted Pair
        PHYAD: 0
        Transceiver: external
        MDI-X: Unknown
        Supports Wake-on: ubgs
        Wake-on: d
        SecureOn password: 00:00:00:00:00:00
        Current message level: 0x000020f7 (8439)
                               drv probe link ifdown ifup rx_err tx_err hw
        Link detected: yes
root@am62axx-evm:/# dmesg | grep eth0
[   12.785425] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[   12.794859] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[   16.902798] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[   16.911705] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
[  528.891258] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
[  532.646647] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[  532.656002] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
[  535.751030] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[  535.759926] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
root@am62axx-evm:/# ip addr show
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host
       valid_lft forever preferred_lft forever
2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether 1c:63:49:1e:8e:e8 brd ff:ff:ff:ff:ff:ff
    inet6 fe80::1e63:49ff:fe1e:8ee8/64 scope link
       valid_lft forever preferred_lft forever
root@am62axx-evm:/# ip link set eth0 down
[ 1707.172161] am65-cpsw-nuss 8000000.ethernet eth0: Link is Down
root@am62axx-evm:/# ip link set eth0 up
[ 1712.939098] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
[ 1712.948452] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
root@am62axx-evm:/#
[ 1716.039140] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[ 1716.048038] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
root@am62axx-evm:/# ip addr show
1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
    link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
    inet 127.0.0.1/8 scope host lo
       valid_lft forever preferred_lft forever
    inet6 ::1/128 scope host
       valid_lft forever preferred_lft forever
2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
    link/ether 1c:63:49:1e:8e:e8 brd ff:ff:ff:ff:ff:ff
    inet6 fe80::1e63:49ff:fe1e:8ee8/64 scope link
       valid_lft forever preferred_lft forever
root@am62axx-evm:/# udhcpc
udhcpc: started, v1.35.0
udhcpc: broadcasting discover
udhcpc: broadcasting discover
udhcpc: broadcasting discover
udhcpc: broadcasting discover
udhcpc: broadcasting discover
udhcpc: broadcasting discover
^C

root@am62axx-evm:/# systemctl list-unit-files --state=enabled
UNIT FILE                            STATE   VENDOR PRESET
atd.service                          enabled enabled
avahi-daemon.service                 enabled enabled
bluetooth.service                    enabled enabled
bt-enable.service                    enabled enabled
containerd.service                   enabled enabled
crond.service                        enabled enabled
dbus-broker.service                  enabled enabled
edgeai-init.service                  enabled enabled
getty@.service                       enabled enabled
gplv3-notice.service                 enabled enabled
ip6tables.service                    enabled enabled
iptables.service                     enabled enabled
irqbalanced.service                  enabled enabled
kdump.service                        enabled enabled
netserver.service                    enabled enabled
nfs-statd.service                    enabled enabled
ofono.service                        enabled enabled
psplash-start.service                enabled enabled
psplash-systemd.service              enabled enabled
resize_rootfs.service                enabled enabled
rpcbind.service                      enabled enabled
strongswan-starter.service           enabled enabled
sync-clocks.service                  enabled disabled
systemd-network-generator.service    enabled enabled
systemd-networkd-wait-online.service enabled disabled
systemd-networkd.service             enabled enabled
systemd-pstore.service               enabled enabled
systemd-resolved.service             enabled enabled
systemd-timesyncd.service            enabled enabled
tee-supplicant.service               enabled enabled
var-volatile-cache.service           enabled enabled
var-volatile-lib.service             enabled enabled
var-volatile-spool.service           enabled enabled
var-volatile-srv.service             enabled enabled
weston.service                       enabled enabled
avahi-daemon.socket                  enabled disabled
docker.socket                        enabled enabled
dropbear.socket                      enabled enabled
rpcbind.socket                       enabled enabled
systemd-networkd.socket              enabled disabled
systemd-userdbd.socket               enabled enabled
weston.socket                        enabled enabled
reboot.target                        enabled enabled
remote-fs.target                     enabled enabled
logrotate.timer                      enabled enabled

45 unit files listed.

The ethernet jack is showing a solid green LED on the right and the left LED blinks on and off occasionally every second with some slight variation.

Is it possible the an Ethernet PHY register was written to disable sending data out?

Thank you for your assistance.

  • As another data point, if I set the IP address to static, I am able to ping to and from it at least:

    root@am62axx-evm:/# ip addr add 192.168.10.2/24 brd + dev eth0
    root@am62axx-evm:/# ip link set eth0 up
    root@am62axx-evm:/# ip addr show
    1: lo: <LOOPBACK,UP,LOWER_UP> mtu 65536 qdisc noqueue state UNKNOWN group default qlen 1000
        link/loopback 00:00:00:00:00:00 brd 00:00:00:00:00:00
        inet 127.0.0.1/8 scope host lo
           valid_lft forever preferred_lft forever
        inet6 ::1/128 scope host
           valid_lft forever preferred_lft forever
    2: eth0: <BROADCAST,MULTICAST,UP,LOWER_UP> mtu 1500 qdisc mq state UP group default qlen 1000
        link/ether 1c:63:49:1e:8e:e8 brd ff:ff:ff:ff:ff:ff
        inet 192.168.10.2/24 brd 192.168.10.255 scope global eth0
           valid_lft forever preferred_lft forever
        inet6 fe80::1e63:49ff:fe1e:8ee8/64 scope link
           valid_lft forever preferred_lft forever
    root@am62axx-evm:/# ping 192.168.10.136
    PING 192.168.10.136 (192.168.10.136): 56 data bytes
    64 bytes from 192.168.10.136: seq=0 ttl=64 time=0.560 ms
    64 bytes from 192.168.10.136: seq=1 ttl=64 time=0.564 ms
    64 bytes from 192.168.10.136: seq=2 ttl=64 time=0.518 ms
    64 bytes from 192.168.10.136: seq=3 ttl=64 time=0.538 ms
    ^C
    

  • But I'm unable to SSH to it, even after manually starting dropbear:

    root@am62axx-evm:/# systemctl status dropbear
    * dropbear.service - LSB: Dropbear Secure Shell server
    Loaded: loaded (/etc/init.d/dropbear; generated)
    Active: inactive (dead)
    Docs: man:systemd-sysv-generator(8)

    root@am62axx-evm:/# systemctl status dropbear
    * dropbear.service - LSB: Dropbear Secure Shell server
    Loaded: loaded (/etc/init.d/dropbear; generated)
    Active: active (running) since Thu 2022-04-28 19:11:32 UTC; 45s ago
    Docs: man:systemd-sysv-generator(8)
    Process: 1715 ExecStart=/etc/init.d/dropbear start (code=exited, status=0/SUCCESS)
    Tasks: 2 (limit: 3290)
    Memory: 728.0K
    CGroup: /system.slice/dropbear.service
    |- 1720 /usr/sbin/dropbear -r /etc/dropbear/dropbear_rsa_host_key -p 22 -B
    `- 1723 /usr/sbin/dropbear -r /etc/dropbear/dropbear_rsa_host_key -p 22 -B

    Apr 28 19:11:30 am62axx-evm systemd[1]: Starting LSB: Dropbear Secure Shell server...
    Apr 28 19:11:30 am62axx-evm dropbear[1715]: Starting Dropbear SSH server:
    Apr 28 19:11:30 am62axx-evm dropbear[1718]: Generating 2048 bit rsa key, this may take a while...
    Apr 28 19:11:32 am62axx-evm dropbear[1718]: Public key portion is:
    Apr 28 19:11:32 am62axx-evm dropbear[1718]: ssh-rsa AAAAB3NzaC1yc2EAAAADAQABAAABAQCcfV4acfvfIpEkxbBLLX+pYAklFsrZVmAmEVF8z1Z8/qQBFUxh0oVWdg9I5GHyaX6HgnFP7RdlKNj>
    Apr 28 19:11:32 am62axx-evm dropbear[1718]: Fingerprint: sha1!! 2a:e9:4c:d1:4b:6f:7b:45:51:63:b1:bb:1b:c3:67:43:0e:2b:09:43
    Apr 28 19:11:32 am62axx-evm dropbear[1720]: Running in background
    Apr 28 19:11:32 am62axx-evm dropbear[1715]: dropbear.
    Apr 28 19:11:32 am62axx-evm systemd[1]: Started LSB: Dropbear Secure Shell server.
    Apr 28 19:12:02 am62axx-evm dropbear[1723]: Child connection from 192.168.10.133:63836

    Using Putty, I just get a blank window and it never prompts me for an authentication key.

  • Additionally here is the boot log:

    U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    am62a_init: board_init_f done
    SPL initial stack usage: 17040 bytes
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Trying to boot from MMC2
    mmc_load_image_raw_sector: mmc block read error
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    Starting ATF on ARM64 core...
    
    NOTICE:  BL31: v2.9(release):v2.9.0-614-gd7a7135d32-dirty
    NOTICE:  BL31: Built : 09:34:15, Aug 24 2023
    
    U-Boot SPL 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    SYSFW ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    am62a_init: board_init_f done
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Trying to boot from MMC2
    mmc_load_image_raw_sector: mmc block read error
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    am62a_init: spl_boot_device: devstat = 0x2c2 bootmedia = 0x8 bootindex = 0
    Authentication passed
    
    
    U-Boot 2023.04-gb0d717b732 (Dec 06 2023 - 15:11:45 +0000)
    
    SoC:   AM62AX SR1.0 HS-FS
    Model: Texas Instruments AM62A7 SK
    DRAM:  2 GiB (effective 4 GiB)
    Core:  58 devices, 28 uclasses, devicetree: separate
    MMC:   mmc@fa10000: 0, mmc@fa00000: 1
    Loading Environment from nowhere... OK
    In:    serial@2800000
    Out:   serial@2800000
    Err:   serial@2800000
    Net:   eth0: ethernet@8000000port@1
    Hit any key to stop autoboot:  0
    switch to partitions #0, OK
    mmc1 is current device
    SD/MMC found on device 1
    Failed to load 'boot.scr'
    639 bytes read in 21 ms (29.3 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc1 ...
    ## Error: "main_cpsw0_qsgmii_phyinit" not defined
    20302336 bytes read in 835 ms (23.2 MiB/s)
    57364 bytes read in 27 ms (2 MiB/s)
    Working FDT set to 88000000
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
    Working FDT set to 88000000
       Loading Device Tree to 000000008feee000, end 000000008fffffff ... OK
    Working FDT set to 8feee000
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0000000000 [0x410fd034]
    [    0.000000] Linux version 6.1.46-g247b2535b2 (oe-user@oe-host) (aarch64-oe-linux-gcc (GCC) 11.4.0, GNU ld (GNU Binutils) 2.38.20220708) #1 SMP PREEMPT Wed Dec  6 17:54:04 UTC 2023
    [    0.000000] Machine model: Texas Instruments AM62A7 SK
    [    0.000000] earlycon: ns16550a0 at MMIO32 0x0000000002800000 (options '')
    [    0.000000] printk: bootconsole [ns16550a0] enabled
    [    0.000000] efi: UEFI not found.
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000c0000000, size 576 MiB
    [    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000099800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node c7x-dma-memory@99800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000099900000, size 30 MiB
    [    0.000000] OF: reserved mem: initialized node c7x-memory@99900000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009b800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009b900000, size 15 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9b900000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c800000, size 1 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x000000009c900000, size 30 MiB
    [    0.000000] OF: reserved mem: initialized node r5f-dma-memory@9c900000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a1000000, size 32 MiB
    [    0.000000] OF: reserved mem: initialized node edgeai-dma-memory@a1000000, compatible id shared-dma-pool
    [    0.000000] OF: reserved mem: initialized node edgeai_shared-memories, compatible id dma-heap-carveout
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000ae000000, size 288 MiB
    [    0.000000] OF: reserved mem: initialized node edgeai-core-heap-memory@ae000000, compatible id shared-dma-pool
    [    0.000000] Zone ranges:
    [    0.000000]   DMA      [mem 0x0000000080000000-0x00000000ffffffff]
    [    0.000000]   DMA32    empty
    [    0.000000]   Normal   [mem 0x0000000100000000-0x00000008ffffffff]
    [    0.000000] Movable zone start for each node
    [    0.000000] Early memory node ranges
    [    0.000000]   node   0: [mem 0x0000000080000000-0x00000000997fffff]
    [    0.000000]   node   0: [mem 0x0000000099800000-0x000000009b7fefff]
    [    0.000000]   node   0: [mem 0x000000009b800000-0x000000009e6fffff]
    [    0.000000]   node   0: [mem 0x000000009e700000-0x000000009e77ffff]
    [    0.000000]   node   0: [mem 0x000000009e780000-0x00000000a2ffffff]
    [    0.000000]   node   0: [mem 0x00000000a3000000-0x00000000adffffff]
    [    0.000000]   node   0: [mem 0x00000000ae000000-0x00000000bfffffff]
    [    0.000000]   node   0: [mem 0x00000000c0000000-0x00000000ffffffff]
    [    0.000000]   node   0: [mem 0x0000000880000000-0x00000008ffffffff]
    [    0.000000] Initmem setup node 0 [mem 0x0000000080000000-0x00000008ffffffff]
    [    0.000000] On node 0, zone DMA: 1 pages in unavailable ranges
    [    0.000000] psci: probing for conduit method from DT.
    [    0.000000] psci: PSCIv1.1 detected in firmware.
    [    0.000000] psci: Using standard PSCI v0.2 function IDs
    [    0.000000] psci: Trusted OS migration not required
    [    0.000000] psci: SMC Calling Convention v1.4
    [    0.000000] percpu: Embedded 19 pages/cpu s37992 r8192 d31640 u77824
    [    0.000000] Detected VIPT I-cache on CPU0
    [    0.000000] CPU features: detected: GIC system register CPU interface
    [    0.000000] CPU features: detected: ARM erratum 845719
    [    0.000000] alternatives: applying boot alternatives
    [    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 1032191
    [    0.000000] Kernel command line: console=ttyS2,115200n8 earlycon=ns16550a,mmio32,0x02800000 mtdparts=spi-nand0:512k(ospi_nand.tiboot3),2m(ospi_nand.tispl),4m(ospi_nand.u-boot),256k(ospi_nand.env),256k(ospi_nand.env.backup),98048k@32m(ospi_nand.rootfs),256k@130816k(ospi_nand.phypattern) root=PARTUUID=83c21bb6-02 rw rootfstype=ext4 rootwait
    [    0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes, linear)
    [    0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes, linear)
    [    0.000000] mem auto-init: stack:off, heap alloc:off, heap free:off
    [    0.000000] software IO TLB: area num 4.
    [    0.000000] software IO TLB: mapped [mem 0x00000000fbfff000-0x00000000fffff000] (64MB)
    [    0.000000] Memory: 2807964K/4194300K available (12288K kernel code, 1266K rwdata, 4020K rodata, 2112K init, 438K bss, 796512K reserved, 589824K cma-reserved)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
    [    0.000000] rcu: Preemptible hierarchical RCU implementation.
    [    0.000000] rcu:     RCU event tracing is enabled.
    [    0.000000] rcu:     RCU restricting CPUs from NR_CPUS=256 to nr_cpu_ids=4.
    [    0.000000]  Trampoline variant of Tasks RCU enabled.
    [    0.000000]  Tracing variant of Tasks RCU enabled.
    [    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 25 jiffies.
    [    0.000000] rcu: Adjusting geometry for rcu_fanout_leaf=16, nr_cpu_ids=4
    [    0.000000] NR_IRQS: 64, nr_irqs: 64, preallocated irqs: 0
    [    0.000000] GICv3: GIC: Using split EOI/Deactivate mode
    [    0.000000] GICv3: 256 SPIs implemented
    [    0.000000] GICv3: 0 Extended SPIs implemented
    [    0.000000] Root IRQ handler: gic_handle_irq
    [    0.000000] GICv3: GICv3 features: 16 PPIs
    [    0.000000] GICv3: CPU0: found redistributor 0 region 0:0x0000000001880000
    [    0.000000] ITS [mem 0x01820000-0x0182ffff]
    [    0.000000] GIC: enabling workaround for ITS: Socionext Synquacer pre-ITS
    [    0.000000] ITS@0x0000000001820000: Devices Table too large, reduce ids 20->19
    [    0.000000] ITS@0x0000000001820000: allocated 524288 Devices @880800000 (flat, esz 8, psz 64K, shr 0)
    [    0.000000] ITS: using cache flushing for cmd queue
    [    0.000000] GICv3: using LPI property table @0x0000000880040000
    [    0.000000] GIC: using cache flushing for LPI property table
    [    0.000000] GICv3: CPU0: using allocated LPI pending table @0x0000000880050000
    [    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
    [    0.000000] arch_timer: cp15 timer(s) running at 200.00MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0x3ffffffffffffff max_cycles: 0x2e2049d3e8, max_idle_ns: 440795210634 ns
    [    0.000000] sched_clock: 58 bits at 200MHz, resolution 5ns, wraps every 4398046511102ns
    [    0.008500] Console: colour dummy device 80x25
    [    0.013087] Calibrating delay loop (skipped), value calculated using timer frequency.. 400.00 BogoMIPS (lpj=800000)
    [    0.023768] pid_max: default: 32768 minimum: 301
    [    0.028535] LSM: Security Framework initializing
    [    0.033358] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.040938] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes, linear)
    [    0.050405] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.057840] cblist_init_generic: Setting shift to 2 and lim to 1.
    [    0.064129] cblist_init_generic: Setting adjustable number of callback queues.
    [    0.071524] cblist_init_generic: Setting shift to 2 and lim to 1.
    [    0.077898] rcu: Hierarchical SRCU implementation.
    [    0.082803] rcu:     Max phase no-delay instances is 1000.
    [    0.088368] Platform MSI: msi-controller@1820000 domain created
    [    0.094626] PCI/MSI: /bus@f0000/interrupt-controller@1800000/msi-controller@1820000 domain created
    [    0.104025] EFI services will not be available.
    [    0.108884] smp: Bringing up secondary CPUs ...
    [    0.114081] Detected VIPT I-cache on CPU1
    [    0.114166] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000
    [    0.114182] GICv3: CPU1: using allocated LPI pending table @0x0000000880060000
    [    0.114225] CPU1: Booted secondary processor 0x0000000001 [0x410fd034]
    [    0.114832] Detected VIPT I-cache on CPU2
    [    0.114902] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000
    [    0.114915] GICv3: CPU2: using allocated LPI pending table @0x0000000880070000
    [    0.114947] CPU2: Booted secondary processor 0x0000000002 [0x410fd034]
    [    0.115503] Detected VIPT I-cache on CPU3
    [    0.115575] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000
    [    0.115588] GICv3: CPU3: using allocated LPI pending table @0x0000000880080000
    [    0.115615] CPU3: Booted secondary processor 0x0000000003 [0x410fd034]
    [    0.115678] smp: Brought up 1 node, 4 CPUs
    [    0.195399] SMP: Total of 4 processors activated.
    [    0.200211] CPU features: detected: 32-bit EL0 Support
    [    0.205480] CPU features: detected: CRC32 instructions
    [    0.210785] CPU: All CPU(s) started at EL2
    [    0.214984] alternatives: applying system-wide alternatives
    [    0.222117] devtmpfs: initialized
    [    0.233626] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns
    [    0.243615] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
    [    0.264172] pinctrl core: initialized pinctrl subsystem
    [    0.270050] DMI not present or invalid.
    [    0.274522] NET: Registered PF_NETLINK/PF_ROUTE protocol family
    [    0.281468] DMA: preallocated 512 KiB GFP_KERNEL pool for atomic allocations
    [    0.288914] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA pool for atomic allocations
    [    0.296997] DMA: preallocated 512 KiB GFP_KERNEL|GFP_DMA32 pool for atomic allocations
    [    0.305157] audit: initializing netlink subsys (disabled)
    [    0.310806] audit: type=2000 audit(0.204:1): state=initialized audit_enabled=0 res=1
    [    0.311188] thermal_sys: Registered thermal governor 'step_wise'
    [    0.318736] thermal_sys: Registered thermal governor 'power_allocator'
    [    0.324914] cpuidle: using governor menu
    [    0.335744] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers.
    [    0.342762] ASID allocator initialised with 65536 entries
    [    0.359276] platform 30200000.dss: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [    0.370583] platform connector: Fixed dependency cycle(s) with /bus@f0000/i2c@20010000/sii9022@3b
    [    0.380051] KASLR disabled due to lack of seed
    [    0.391090] HugeTLB: registered 1.00 GiB page size, pre-allocated 0 pages
    [    0.398051] HugeTLB: 0 KiB vmemmap can be freed for a 1.00 GiB page
    [    0.404460] HugeTLB: registered 32.0 MiB page size, pre-allocated 0 pages
    [    0.411400] HugeTLB: 0 KiB vmemmap can be freed for a 32.0 MiB page
    [    0.417809] HugeTLB: registered 2.00 MiB page size, pre-allocated 0 pages
    [    0.424749] HugeTLB: 0 KiB vmemmap can be freed for a 2.00 MiB page
    [    0.431156] HugeTLB: registered 64.0 KiB page size, pre-allocated 0 pages
    [    0.438096] HugeTLB: 0 KiB vmemmap can be freed for a 64.0 KiB page
    [    0.445780] k3-chipinfo 43000014.chipid: Family:AM62AX rev:SR1.0 JTAGID[0x0bb8d02f] Detected
    [    0.455877] iommu: Default domain type: Translated
    [    0.460891] iommu: DMA domain TLB invalidation policy: strict mode
    [    0.467544] SCSI subsystem initialized
    [    0.471658] usbcore: registered new interface driver usbfs
    [    0.477303] usbcore: registered new interface driver hub
    [    0.482758] usbcore: registered new device driver usb
    [    0.488313] pps_core: LinuxPPS API ver. 1 registered
    [    0.493392] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.502740] PTP clock support registered
    [    0.506874] EDAC MC: Ver: 3.0.0
    [    0.510842] omap-mailbox 29000000.mailbox: omap mailbox rev 0x66fca100
    [    0.517668] omap-mailbox 29010000.mailbox: omap mailbox rev 0x66fca100
    [    0.524471] omap-mailbox 29020000.mailbox: omap mailbox rev 0x66fca100
    [    0.531200] omap-mailbox 29030000.mailbox: no available mbox devices found
    [    0.538506] FPGA manager framework
    [    0.542052] Advanced Linux Sound Architecture Driver Initialized.
    [    0.549118] clocksource: Switched to clocksource arch_sys_counter
    [    0.555563] VFS: Disk quotas dquot_6.6.0
    [    0.559613] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes)
    [    0.572391] Carveout Heap: Exported 176 MiB at 0x00000000a3000000
    [    0.578738] NET: Registered PF_INET protocol family
    [    0.583917] IP idents hash table entries: 65536 (order: 7, 524288 bytes, linear)
    [    0.594353] tcp_listen_portaddr_hash hash table entries: 2048 (order: 3, 32768 bytes, linear)
    [    0.603159] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
    [    0.611101] TCP established hash table entries: 32768 (order: 6, 262144 bytes, linear)
    [    0.619407] TCP bind hash table entries: 32768 (order: 8, 1048576 bytes, linear)
    [    0.627774] TCP: Hash tables configured (established 32768 bind 32768)
    [    0.634633] UDP hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.641593] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes, linear)
    [    0.649118] NET: Registered PF_UNIX/PF_LOCAL protocol family
    [    0.655272] RPC: Registered named UNIX socket transport module.
    [    0.661344] RPC: Registered udp transport module.
    [    0.666154] RPC: Registered tcp transport module.
    [    0.670962] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.677552] NET: Registered PF_XDP protocol family
    [    0.682461] PCI: CLS 0 bytes, default 64
    [    0.687086] hw perfevents: enabled with armv8_cortex_a53 PMU driver, 7 counters available
    [    0.696954] Initialise system trusted keyrings
    [    0.701719] workingset: timestamp_bits=46 max_order=20 bucket_order=0
    [    0.712621] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.719131] NFS: Registering the id_resolver key type
    [    0.724349] Key type id_resolver registered
    [    0.728629] Key type id_legacy registered
    [    0.732779] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
    [    0.739635] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
    [    0.782961] Key type asymmetric registered
    [    0.787155] Asymmetric key parser 'x509' registered
    [    0.792182] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 245)
    [    0.799883] io scheduler mq-deadline registered
    [    0.804522] io scheduler kyber registered
    [    0.811582] pinctrl-single 4084000.pinctrl: 34 pins, size 136
    [    0.818016] pinctrl-single f4000.pinctrl: 151 pins, size 604
    [    0.824850] pinctrl-single a40000.pinctrl: 512 pins, size 2048
    [    0.836765] Serial: 8250/16550 driver, 12 ports, IRQ sharing enabled
    [    0.851875] loop: module loaded
    [    0.856250] megasas: 07.719.03.00-rc1
    [    0.862865] tun: Universal TUN/TAP device driver, 1.6
    [    0.868755] thunder_xcv, ver 1.0
    [    0.872097] thunder_bgx, ver 1.0
    [    0.875422] nicpf, ver 1.0
    [    0.878351] e1000: Intel(R) PRO/1000 Network Driver
    [    0.883338] e1000: Copyright (c) 1999-2006 Intel Corporation.
    [    0.889247] e1000e: Intel(R) PRO/1000 Network Driver
    [    0.894323] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
    [    0.900406] igb: Intel(R) Gigabit Ethernet Network Driver
    [    0.905925] igb: Copyright (c) 2007-2014 Intel Corporation.
    [    0.911653] igbvf: Intel(R) Gigabit Virtual Function Network Driver
    [    0.918061] igbvf: Copyright (c) 2009 - 2012 Intel Corporation.
    [    0.924228] sky2: driver version 1.30
    [    0.928646] VFIO - User Level meta-driver version: 0.3
    [    0.934567] usbcore: registered new interface driver usb-storage
    [    0.941249] i2c_dev: i2c /dev entries driver
    [    0.946977] sdhci: Secure Digital Host Controller Interface driver
    [    0.953324] sdhci: Copyright(c) Pierre Ossman
    [    0.957982] sdhci-pltfm: SDHCI platform and OF driver helper
    [    0.964499] ledtrig-cpu: registered to indicate activity on CPUs
    [    0.970825] SMCCC: SOC_ID: ARCH_SOC_ID not implemented, skipping ....
    [    0.977760] usbcore: registered new interface driver usbhid
    [    0.983462] usbhid: USB HID core driver
    [    0.988222] optee: probing for conduit method.
    [    0.992804] optee: revision 4.0 (2a5b1d12)
    [    0.993061] optee: dynamic shared memory is enabled
    [    1.002599] optee: initialized driver
    [    1.007781] Initializing XFRM netlink socket
    [    1.012193] NET: Registered PF_PACKET protocol family
    [    1.017420] Key type dns_resolver registered
    [    1.022144] registered taskstats version 1
    [    1.026358] Loading compiled-in X.509 certificates
    [    1.039299] ti-sci 44043000.system-controller: ABI: 3.1 (firmware rev 0x0009 '9.1.8--v09.01.08 (Kool Koala)')
    [    1.079615] omap_i2c 20000000.i2c: bus 0 rev0.12 at 400 kHz
    [    1.086630] pca953x 1-0023: supply vcc not found, using dummy regulator
    [    1.093516] pca953x 1-0023: using AI
    [    1.123673] omap_i2c 20010000.i2c: bus 1 rev0.12 at 100 kHz
    [    1.130425] omap_i2c 20020000.i2c: bus 2 rev0.12 at 400 kHz
    [    1.136355] ti-sci-intr 4210000.interrupt-controller: Interrupt Router 5 domain created
    [    1.144682] ti-sci-intr bus@f0000:interrupt-controller@a00000: Interrupt Router 3 domain created
    [    1.153881] ti-sci-inta 48000000.interrupt-controller: Interrupt Aggregator domain 28 created
    [    1.162870] ti-sci-inta 4e0a0000.interrupt-controller: Interrupt Aggregator domain 200 created
    [    1.172572] ti-udma 485c0100.dma-controller: Number of rings: 82
    [    1.180633] ti-udma 485c0100.dma-controller: Channels: 48 (bchan: 18, tchan: 12, rchan: 18)
    [    1.191473] ti-udma 485c0000.dma-controller: Number of rings: 150
    [    1.201304] ti-udma 485c0000.dma-controller: Channels: 35 (tchan: 20, rchan: 15)
    [    1.210627] ti-udma 4e230000.dma-controller: Number of rings: 6
    [    1.217096] ti-udma 4e230000.dma-controller: Channels: 6 (bchan: 0, tchan: 0, rchan: 6)
    [    1.226308] printk: console [ttyS2] disabled
    [    1.230739] 2800000.serial: ttyS2 at MMIO 0x2800000 (irq = 253, base_baud = 3000000) is a 8250
    [    1.239616] printk: console [ttyS2] enabled
    [    1.239616] printk: console [ttyS2] enabled
    [    1.248077] printk: bootconsole [ns16550a0] disabled
    [    1.248077] printk: bootconsole [ns16550a0] disabled
    [    1.260260] spi-nand spi0.0: Winbond SPI NAND was found.
    [    1.265597] spi-nand spi0.0: 128 MiB, block size: 256 KiB, page size: 4096, OOB size: 128
    [    1.273950] 7 fixed-partitions partitions found on MTD device spi0.0
    [    1.280307] Creating 7 MTD partitions on "spi0.0":
    [    1.285094] 0x000000000000-0x000000080000 : "ospi_nand.tiboot3"
    [    1.292313] 0x000000080000-0x000000280000 : "ospi_nand.tispl"
    [    1.299882] 0x000000280000-0x000000680000 : "ospi_nand.u-boot"
    [    1.308292] 0x000000680000-0x0000006c0000 : "ospi_nand.env"
    [    1.314970] 0x0000006c0000-0x000000700000 : "ospi_nand.env.backup"
    [    1.322245] 0x000002000000-0x000007fc0000 : "ospi_nand.rootfs"
    [    1.366657] 0x000007fc0000-0x000008000000 : "ospi_nand.phypattern"
    [    1.413158] davinci_mdio 8000f00.mdio: davinci mdio revision 9.7, bus freq 1000000
    [    1.422228] davinci_mdio 8000f00.mdio: phy[0]: device 8000f00.mdio:00, driver TI DP83867
    [    1.430362] am65-cpsw-nuss 8000000.ethernet: initializing am65 cpsw nuss version 0x6BA01103, cpsw version 0x6BA81103 Ports: 3 quirks:00000006
    [    1.443135] am65-cpsw-nuss 8000000.ethernet: initialized cpsw ale version 1.5
    [    1.450263] am65-cpsw-nuss 8000000.ethernet: ALE Table size 512
    [    1.456601] pps pps0: new PPS source ptp0
    [    1.460863] am65-cpsw-nuss 8000000.ethernet: CPTS ver 0x4e8a010c, freq:500000000, add_val:1 pps:1
    [    1.471115] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19
    [    1.479461] cpufreq: cpufreq_online: CPU0: Running at unlisted initial frequency: 1200000 KHz, changing to: 1250000 KHz
    [    1.491787] mmc0: CQHCI version 5.10
    [    1.536599] mmc0: SDHCI controller on fa10000.mmc [fa10000.mmc] using ADMA 64-bit
    [    1.626941] mmc0: Command Queue Engine enabled
    [    1.631460] mmc0: new HS200 MMC card at address 0001
    [    1.637205] mmcblk0: mmc0:0001 G1M15L 29.6 GiB
    [    1.645195]  mmcblk0: p1 p2
    [    1.648674] mmcblk0boot0: mmc0:0001 G1M15L 31.5 MiB
    [    1.654759] mmcblk0boot1: mmc0:0001 G1M15L 31.5 MiB
    [    1.660536] mmcblk0rpmb: mmc0:0001 G1M15L 4.00 MiB, chardev (240:0)
    [    1.810623] tps6594-rtc tps6594-rtc.4.auto: registered as rtc0
    [    1.816635] tps6594-rtc tps6594-rtc.4.auto: hctosys: unable to read the hardware clock
    [    1.826247] pca953x 1-0022: supply vcc not found, using dummy regulator
    [    1.833349] pca953x 1-0022: using AI
    [    1.843374] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
    [    1.850990] mmc1: CQHCI version 5.10
    [    1.851825] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
    [    1.861932] debugfs: Directory 'pd:182' with parent 'pm_genpd' already present!
    [    1.875180] ALSA device list:
    [    1.878182]   No soundcards found.
    [    1.895810] mmc1: SDHCI controller on fa00000.mmc [fa00000.mmc] using ADMA 64-bit
    [    1.903475] Waiting for root device PARTUUID=83c21bb6-02...
    [    1.967586] mmc1: new ultra high speed SDR104 SDHC card at address b368
    [    1.975553] mmcblk1: mmc1:b368 LX32G 29.5 GiB
    [    1.983437]  mmcblk1: p1 p2
    [    2.046090] EXT4-fs (mmcblk1p2): mounted filesystem with ordered data mode. Quota mode: none.
    [    2.054719] VFS: Mounted root (ext4 filesystem) on device 179:98.
    [    2.062187] devtmpfs: mounted
    [    2.065881] Freeing unused kernel memory: 2112K
    [    2.070506] Run /sbin/init as init process
    [    2.265456] systemd[1]: System time before build time, advancing clock.
    [    2.324485] NET: Registered PF_INET6 protocol family
    [    2.331107] Segment Routing with IPv6
    [    2.334875] In-situ OAM (IOAM) with IPv6
    [    2.372944] systemd[1]: systemd 250.5+ running in system mode (+PAM -AUDIT -SELINUX -APPARMOR +IMA -SMACK +SECCOMP -GCRYPT -GNUTLS -OPENSSL +ACL +BLKID -CURL -ELFUTILS -FIDO2 -IDN2 -IDN -IPTC +KMOD -LIBCRYPTSETUP +LIBFDISK -PCRE2 -PWQUALITY -P11KIT -QRENCODE -BZIP2 -LZ4 -XZ -ZLIB +ZSTD -BPF_FRAMEWORK +XKBCOMMON +UTMP +SYSVINIT default-hierarchy=hybrid)
    [    2.404983] systemd[1]: Detected architecture arm64.
    
    Welcome to Arago 2023.10!
    
    [    2.482510] systemd[1]: Hostname set to <am62axx-evm>.
    [    2.591170] systemd-sysv-generator[159]: SysV service '/etc/init.d/netopeer2-server' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.616698] systemd-sysv-generator[159]: SysV service '/etc/init.d/edgeai-launcher.sh' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.642370] systemd-sysv-generator[159]: SysV service '/etc/init.d/thermal-zone-init' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.668915] systemd-sysv-generator[159]: SysV service '/etc/init.d/sysrepo' lacks a native systemd unit file. Automatically generating a unit file for compatibility. Please update package to include a native systemd unit file, in order to make it more safe and robust.
    [    2.964587] systemd[1]: /lib/systemd/system/bt-enable.service:9: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.031645] systemd[1]: /etc/systemd/system/sync-clocks.service:11: Standard output type syslog is obsolete, automatically updating to journal. Please update your unit file, and consider removing the setting altogether.
    [    3.108977] systemd[1]: Queued start job for default target Graphical Interface.
    [    3.183482] systemd[1]: Created slice Slice /system/getty.
    [  OK  ] Created slice Slice /system/getty.
    [    3.208339] systemd[1]: Created slice Slice /system/modprobe.
    [  OK  ] Created slice Slice /system/modprobe.
    [    3.232416] systemd[1]: Created slice Slice /system/serial-getty.
    [  OK  ] Created slice Slice /system/serial-getty.
    [    3.256140] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    3.277795] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password …ts to Console Directory Watch.
    [    3.301661] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password R…uests to Wall Directory Watch.
    [    3.326197] systemd[1]: Reached target Path Units.
    [  OK  ] Reached target Path Units.
    [    3.341452] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    3.361453] systemd[1]: Reached target Slice Units.
    [  OK  ] Reached target Slice Units.
    [    3.377429] systemd[1]: Reached target Swaps.
    [  OK  ] Reached target Swaps.
    [    3.446860] systemd[1]: Listening on RPCbind Server Activation Socket.
    [  OK  ] Listening on RPCbind Server Activation Socket.
    [    3.469754] systemd[1]: Reached target RPC Port Mapper.
    [  OK  ] Reached target RPC Port Mapper.
    [    3.508319] systemd[1]: Listening on Process Core Dump Socket.
    [  OK  ] Listening on Process Core Dump Socket.
    [    3.530085] systemd[1]: Listening on initctl Compatibility Named Pipe.
    [  OK  ] Listening on initctl Compatibility Named Pipe.
    [    3.556846] systemd[1]: Listening on Journal Audit Socket.
    [  OK  ] Listening on Journal Audit Socket.
    [    3.579842] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    3.603961] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    3.624890] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    3.652227] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    3.675308] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    3.699702] systemd[1]: Listening on User Database Manager Socket.
    [  OK  ] Listening on User Database Manager Socket.
    [    3.761786] systemd[1]: Mounting Huge Pages File System...
             Mounting Huge Pages File System...
    [    3.783323] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    3.814782] systemd[1]: Mounting Kernel Debug File System...
             Mounting Kernel Debug File System...
    [    3.838539] systemd[1]: Kernel Trace File System was skipped because of a failed condition check (ConditionPathExists=/sys/kernel/tracing).
    [    3.881668] systemd[1]: Mounting Temporary Directory /tmp...
             Mounting Temporary Directory /tmp...
    [    3.905319] systemd[1]: Starting Create List of Static Device Nodes...
             Starting Create List of Static Device Nodes...
    [    3.927581] systemd[1]: Starting Load Kernel Module configfs...
             Starting Load Kernel Module configfs...
    [    3.950616] systemd[1]: Starting Load Kernel Module drm...
             Starting Load Kernel Module drm...
    [    3.970630] systemd[1]: Starting Load Kernel Module fuse...
             Starting Load Kernel Module fuse...
    [    3.992580] fuse: init (API version 7.37)
    [    4.030037] systemd[1]: Starting Start psplash boot splash screen...
             Starting Start psplash boot splash screen...
    [    4.065082] systemd[1]: Starting RPC Bind...
             Starting RPC Bind...
    [    4.081669] systemd[1]: File System Check on Root Device was skipped because of a failed condition check (ConditionPathIsReadWrite=!/).
    [    4.126076] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.155380] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.174852] systemd[1]: Starting Generate network units from Kernel command line...
    [    4.175513] cryptodev: loading out-of-tree module taints kernel.
             Starting Generate network …ts from Kernel co[    4.190740] cryptodev: driver 1.12 loaded.
    mmand line...
    [    4.214204] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.233172] EXT4-fs (mmcblk1p2): re-mounted. Quota mode: none.
    [    4.261915] systemd[1]: Starting Coldplug All udev Devices...
             Starting Coldplug All udev Devices...
    [    4.286685] systemd[1]: Started RPC Bind.
    [  OK  ] Started RPC Bind.
    [    4.302221] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Mounted Huge Pages File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [  OK  ] Mounted Kernel Debug File System.
    [  OK  ] Mounted Temporary Directory /tmp.
    [  OK  ] Finished Create List of Static Device Nodes.
    [  OK  ] Finished Load Kernel Module configfs.
    [  OK  ] Finished Load Kernel Module drm.
    [  OK  ] Finished Load Kernel Module fuse.
    [FAILED] Failed to start Start psplash boot splash screen.
    See 'systemctl status psplash-start.service' for details.
    [DEPEND] Dependency failed for Star…progress communication helper.
    [  OK  ] Finished Load Kernel Modules.
    [  OK  ] Finished Generate network units from Kernel command line.
    [  OK  ] Finished Remount Root and Kernel File Systems.
             Mounting FUSE Control File System...
             Mounting Kernel Configuration File System...
             Starting Flush Journal to Persistent Storage...
    [    4.700879] systemd-journald[176]: Received client request to flush runtime journal.
             Starting Apply Kernel Variables...
             Starting Create Static Device Nodes in /dev...
    [  OK  ] Mounted FUSE Control File System.
    [  OK  ] Mounted Kernel Configuration File System.
    [  OK  ] Finished Flush Journal to Persistent Storage.
    [  OK  ] Finished Apply Kernel Variables.
    [  OK  ] Finished Create Static Device Nodes in /dev.
    [  OK  ] Reached target Preparation for Local File Systems.
             Mounting /media/ram...
             Mounting /var/volatile...
    [    4.917822] audit: type=1334 audit(1651167747.652:2): prog-id=5 op=LOAD
    [    4.924676] audit: type=1334 audit(1651167747.660:3): prog-id=6 op=LOAD
             Starting Rule-based Manage…for Device Events and Files...
    [  OK  ] Finished Coldplug All udev Devices.
    [  OK  ] Mounted /media/ram.
    [  OK  ] Mounted /var/volatile.
             Starting Load/Save Random Seed...
    [  OK  ] Reached target Local File Systems.
             Starting Create Volatile Files and Directories...
    [  OK  ] Started Rule-based Manager for Device Events and Files.
    [  OK  ] Finished Create Volatile Files and Directories.
             Starting Network Time Synchronization...
             Starting Record System Boot/Shutdown in UTMP...
    [  OK  ] Finished Record System Boot/Shutdown in UTMP.
    [    5.521435] tlv320aic3x 1-001b: supply DVDD not found, using dummy regulator
    [    5.583228] random: crng init done
    [  OK  ] Finished Load/Save Random Seed.
    [    5.643706] mc: Linux media interface: v0.10
    [  OK  ] Found device /dev/ttyS2.
    [    5.671233] videodev: Linux video capture interface: v2.00
    [    5.712408] k3-dsp-rproc 7e000000.dsp: assigned reserved memory node c7x-dma-memory@99800000
    [    5.721550] k3-dsp-rproc 7e000000.dsp: configured DSP for remoteproc mode
    [    5.740529] remoteproc remoteproc0: 7e000000.dsp is available
    [  OK  ] Started Network Time Synchronization.
    [  OK  ] Reached target System Initialization.
    [    5.817765] remoteproc remoteproc0: powering up 7e000000.dsp
    [    5.823796] remoteproc remoteproc0: Booting fw image am62a-c71_0-fw, size 11046992
    [  OK  ] Started Daily Cleanup of Temporary Directories.
    [    5.845612] k3-dsp-rproc 7e000000.dsp: booting DSP core using boot addr = 0x99a00000
    [  OK  ] Reached target System Time Set.
    [    5.861820] rproc-virtio rproc-virtio.5.auto: assigned reserved memory node c7x-dma-memory@99800000
    [  OK  ] Started Daily rotation of log files[    5.874098] vdec 30210000.video-codec: error -ENXIO: IRQ index 0 not found
    .
    [    5.876704] platform 79000000.r5f: configured R5F for remoteproc mode
    [    5.885816] vdec 30210000.video-codec: failed to get irq resource, falling back to polling
    [    5.892244] platform 79000000.r5f: assigned reserved memory node r5f-dma-memory@9b800000
    [  OK  ] Reached target Timer Units.
    [    5.916602] remoteproc remoteproc1: 79000000.r5f is available
    [    5.929441] remoteproc remoteproc1: powering up 79000000.r5f
    [    5.935379] remoteproc remoteproc1: Booting fw image am62a-mcu-r5f0_0-fw, size 52148
    [  OK  ] Listening on Avahi mDNS/DNS-SD Stac[    5.944727] virtio_rpmsg_bus virtio0: rpmsg host is online
    k Activation Socket.
    [    5.954672] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0xd
    [    5.963674] rtc-ti-k3 2b1f0000.rtc: Clock rate 32552 is not 32768! Could misbehave!
    [    5.963732] platform 78000000.r5f: R5F core may have been powered on by a different host, programmed state (0) != actual state (1)
    [    5.972571] rproc-virtio rproc-virtio.5.auto: registered virtio0 (type 7)
    [    5.990255] remoteproc remoteproc0: remote processor 7e000000.dsp is now up
    [  OK  ] Listening on D-Bus System Message B[    5.997560] rproc-virtio rproc-virtio.6.auto: assigned reserved memory node r5f-dma-memory@9b800000
    us Socket.
    [    6.011902] platform 78000000.r5f: configured R5F for IPC-only mode
    [    6.012045] platform 78000000.r5f: assigned reserved memory node r5f-dma-memory@9c800000
    [    6.029463] remoteproc remoteproc2: 78000000.r5f is available
    [    6.029733] sii902x 1-003b: supply iovcc not found, using dummy regulator
    [    6.035341] remoteproc remoteproc2: attaching to 78000000.r5f
    [    6.042261] sii902x 1-003b: supply cvcc12 not found, using dummy regulator
    [    6.048503] platform 78000000.r5f: R5F core initialized in IPC-only mode
    [    6.061636] rproc-virtio rproc-virtio.7.auto: assigned reserved memory node r5f-dma-memory@9c800000
             Starting Docker Socket for the API...
    [    6.062040] virtio_rpmsg_bus virtio1: rpmsg host is online
    [    6.067754] rtc-ti-k3 2b1f0000.rtc: registered as rtc1
    [    6.087013] rproc-virtio rproc-virtio.6.auto: registered virtio1 (type 7)
    [    6.093969] remoteproc remoteproc1: remote processor 79000000.r5f is now up
    [    6.101220] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd
    [    6.114970] virtio_rpmsg_bus virtio2: rpmsg host is online
    [    6.115569] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0xd
    [    6.121277] rproc-virtio rproc-virtio.7.auto: registered virtio2 (type 7)
    [    6.127697] virtio_rpmsg_bus virtio0: creating channel rpmsg_chrdev addr 0x15
    [    6.129852] i2c i2c-1: Added multiplexed i2c bus 3
    [    6.134368] remoteproc remoteproc2: remote processor 78000000.r5f is now attached
    [    6.153993] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe
    [    6.154740] [drm] Initialized tidss 1.0.0 20180215 for 30200000.dss on minor 0
    [    6.162699] virtio_rpmsg_bus virtio2: creating channel rpmsg_chrdev addr 0x15
    [    6.175896] virtio_rpmsg_bus virtio2: creating channel ti.ipc4.ping-pong addr 0xe
    [    6.189349] virtio_rpmsg_bus virtio0: creating channel ti.ipc4.ping-pong addr 0xe
    [    6.271769] e5010 fd20000.e5010: Device registered as /dev/video2
    [    6.273262] Console: switching to colour frame buffer device 200x56
    [    6.292860] mtdblock: MTD device 'ospi_nand.tiboot3' is NAND, please consider using UBI block devices instead.
    [    6.297461] mtdblock: MTD device 'ospi_nand.tispl' is NAND, please consider using UBI block devices instead.
    [    6.301470] mtdblock: MTD device 'ospi_nand.u-boot' is NAND, please consider using UBI block devices instead.
    [    6.309187] tidss 30200000.dss: [drm] fb0: tidssdrmfb frame buffer device
    [    6.312006] mtdblock: MTD device 'ospi_nand.env' is NAND, please consider using UBI block devices instead.
    [    6.313469] mtdblock: MTD device 'ospi_nand.env.backup' is NAND, please consider using UBI block devices instead.
    [    6.334662] mtdblock: MTD device 'ospi_nand.phypattern' is NAND, please consider using UBI block devices instead.
    [  OK  ] Listening on dropbear.socket.
    [    6.383056] mtdblock: MTD device 'ospi_nand.rootfs' is NAND, please consider using UBI block devices instead.
    [  OK  ] Listening on PC/SC Smart Card Daemon Activation Socket.
             Starting Weston socket...
             Starting Console System Startup Logging...
             Starting D-Bus System Message Bus...
             Starting Reboot and dump vmcore via kexec...
    [  OK  ] Listening on Docker Socket for the API.
    [  OK  ] Listening on Weston socket.
    [  OK  ] Finished Console System Startup Logging.
    [  OK  ] Finished Reboot and dump vmcore via kexec.
    [  OK  ] Reached target Socket Units.
    [  OK  ] Started D-Bus System Message Bus.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started Job spooling tools.
    [  OK  ] Started Periodic Command Scheduler.
             Starting DEMO...
             Starting Print notice about GPLv3 packages...
             Starting IPv6 Packet Filtering Framework...
             Starting IPv4 Packet Filtering Framework...
    [  OK  ] Started irqbalance daemon.
             Starting Telephony service...
             Starting Expand the rootfs…ll size of the boot device....
    [  OK  ] Started strongSwan IPsec I…IKEv2 daemon using ipsec.conf.
    [    6.903342] audit: type=1334 audit(1651169541.848:4): prog-id=7 op=LOAD
    [    6.916182] audit: type=1334 audit(1651169541.860:5): prog-id=8 op=LOAD
             Starting User Login Management...
    [  OK  ] Started TEE Supplicant.
             Starting Telnet Server...
    [  OK  ] Finished IPv6 Packet Filtering Framework.
    [  OK  ] Finished IPv4 Packet Filtering Framework.
    [  OK  ] Finished Telnet Server.
    [  OK  ] Started Telephony service.
    [  OK  ] Started DEMO.
    [    7.112466] Bluetooth: Core ver 2.22
    [    7.116212] NET: Registered PF_BLUETOOTH protocol family
    [    7.121679] Bluetooth: HCI device and connection manager initialized
    [    7.153191] Bluetooth: HCI socket layer initialized
    [    7.163208] Bluetooth: L2CAP socket layer initialized
    [    7.177204] Bluetooth: SCO socket layer initialized
    [    7.216738] tps6598x 0-003f: Unable to find the interrupt, switching to polling
    [  OK  ] Reached target Preparation for Network.
             Starting Network Configuration...
    [  OK  ] Finished Expand the rootfs…full size of the boot device..
    [    7.459425] mtdblock: MTD device 'ospi_nand.phypattern' is NAND, please consider using UBI block devices instead.
    [    7.526834] xhci-hcd xhci-hcd.10.auto: xHCI Host Controller
    [    7.527181] xhci-hcd xhci-hcd.10.auto: new USB bus registered, assigned bus number 1
    [    7.527401] xhci-hcd xhci-hcd.10.auto: USB3 root hub has no ports
    [    7.527416] xhci-hcd xhci-hcd.10.auto: hcc params 0x0258fe6d hci version 0x110 quirks 0x0000000000010010
    [    7.527479] xhci-hcd xhci-hcd.10.auto: irq 543, io mem 0x31100000
    [    7.528927] mtdblock: MTD device 'ospi_nand.env.backup' is NAND, please consider using UBI block devices instead.
    [  OK  ] Reached target Hardware activated USB gadget.
    [    7.610888] mtdblock: MTD device 'ospi_nand.phypattern' is NAND, please consider using UBI block devices instead.
    [  OK  ] Listening on Load/Save RF …itch Status /dev/rfkill Watch.
    [  OK  ] Started User Login Management.
    [    7.720777] mtdblock: MTD device 'ospi_nand.env.backup' is NAND, please consider using UBI block devices instead.
             Starting Save/Restore Sound Card State...
    [    7.769608] hub 1-0:1.0: USB hub found
    [    7.774987] hub 1-0:1.0: 1 port detected
    [  OK  ] Finished Save/Restore Sound Card State.
    [  OK  ] Reached target Sound Card.
    [    7.818001] cdns-csi2rx: probe of 30101000.csi-bridge failed with error -22
    [    7.893326] mtdblock: MTD device 'ospi_nand.u-boot' is NAND, please consider using UBI block devices instead.
    [    7.941955] cfg80211: Loading compiled-in X.509 certificates for regulatory database
    [    7.958974] cfg80211: Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
    [    7.961664] mtdblock: MTD device 'ospi_nand.tiboot3' is NAND, please consider using UBI block devices instead.
    [    7.997737] mtdblock: MTD device 'ospi_nand.rootfs' is NAND, please consider using UBI block devices instead.
    [  OK  ] Started Network Configuration.
             Starting Network Name Resolution...
    [    8.040568] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [TI DP83867] (irq=POLL)
    [    8.053902] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode
    [  OK  ] Started Network Name Resolution.
    [  OK  ] Reached target Network.
    [  OK  ] Reached target Host and Network Name Lookups.
             Starting Avahi mDNS/DNS-SD Stack...
             Starting Enable and configure wl18xx bluetooth stack...
             Starting containerd container runtime...
    [  OK  ] Started Netperf Benchmark Server.
    [  OK  ] Started NFS status monitor for NFSv2/3 locking..
             Starting Simple Network Ma…ent Protocol (SNMP) Daemon....
             Starting Permit User Sessions...
    [  OK  ] Finished Enable and configure wl18xx bluetooth stack.
    [  OK  ] Started Avahi mDNS/DNS-SD Stack.
    [  OK  ] Finished Permit User Sessions.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started Serial Getty on ttyS2.
    [  OK  ] Reached target Login Prompts.
             Starting Synchronize System and HW clocks...
             Starting Weston, a Wayland…ositor, as a system service...
    [    8.716166] audit: type=1334 audit(1651169543.660:6): prog-id=9 op=LOAD
    [    8.722893] audit: type=1334 audit(1651169543.668:7): prog-id=10 op=LOAD
             Starting User Database Manager...
    [    8.807078] mtdblock: MTD device 'ospi_nand.env' is NAND, please consider using UBI block devices instead.
    [    8.837031] mtdblock: MTD device 'ospi_nand.tispl' is NAND, please consider using UBI block devices instead.
    [  OK  ] Started User Database Manager.
    [  OK  ] Created slice User Slice of UID 1000.
             Starting User Runtime Directory /run/user/1000...
    [  OK  ] Finished Synchronize System and HW clocks.
    [  OK  ] Finished User Runtime Directory /run/user/1000.
             Starting User Manager for UID 1000...
    [    9.137537] audit: type=1006 audit(1651169544.084:8): pid=652 uid=0 old-auid=4294967295 auid=1000 tty=(none) old-ses=4294967295 ses=1 res=1
    [    9.150228] audit: type=1300 audit(1651169544.084:8): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=fffffa93a688 a2=4 a3=ffff895fc020 items=0 ppid=1 pid=652 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=1 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [  OK  ] Created slice Slice /system/systemd[    9.179986] audit: type=1327 audit(1651169544.084:8): proctitle="(systemd)"
    -fsck.
    [  OK  ] Found device /dev/mmcblk0p1.
             Starting File System Check on /dev/mmcblk0p1...
    [  OK  ] Started Simple Network Man…ement Protocol (SNMP) Daemon..
    [  OK  ] Finished File System Check on /dev/mmcblk0p1.
             Mounting /run/media/mmcblk0p1...
    [    9.528116] EXT4-fs (mmcblk0p1): mounted filesystem with ordered data mode. Quota mode: none.
    [  OK  ] Mounted /run/media/mmcblk0p1.
    [  OK  ] Found device /dev/mmcblk1p1.
             Starting File System Check on /dev/mmcblk1p1...
    [  OK  ] Finished File System Check on /dev/mmcblk1p1.
             Mounting /run/media/BOOT-mmcblk1p1...
    [  OK  ] Started User Manager for UID 1000.
    [  OK  ] Started Session c1 of User weston.
    [    9.834077] audit: type=1006 audit(1651169544.780:9): pid=620 uid=0 old-auid=4294967295 auid=1000 tty=tty7 old-ses=4294967295 ses=2 res=1
    [    9.846515] audit: type=1300 audit(1651169544.780:9): arch=c00000b7 syscall=64 success=yes exit=4 a0=8 a1=fffffa93a688 a2=4 a3=ffff895fc020 items=0 ppid=1 pid=620 auid=1000 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=tty7 ses=2 comm="(weston)" exe="/lib/systemd/systemd" key=(null)
    [    9.872789] audit: type=1327 audit(1651169544.780:9): proctitle="(weston)"
    [  OK  ] Mounted /run/media/BOOT-mmcblk1p1.
    [  OK  ] Started containerd container runtime.
    [  OK  ] Started Weston, a Wayland …mpositor, as a system service.
             Starting EdgeAI OOB demos...
             Stopping Weston, a Wayland…ositor, as a system service...
    ***************************************************************
    ***************************************************************
    NOTICE: This file system contains the following GPL-3.0 packages:
            adwaita-icon-theme-symbolic
            autoconf
            bash-dev
            bash
            bc
            binutils
            cifs-utils
            coreutils-stdbuf
            coreutils
            cpio
            cpp-symlinks
            cpp
            dosfstools
            elfutils
            g++-symlinks
            g++
            gawk
            gcc-symlinks
            gcc
            gdb
            gdbserver
            gettext
            glmark2
            gnu-config
            grub-common
            grub-editenv
            grub-efi
            gzip
            hidapi
            less
            libasm1
            libatomic-dev
            libatomic1
            libbfd
            libdebuginfod1
            libdw1
            libeigen-dev
            libelf1
            libgcc-s-dev
            libgcc1
            libgdbm-compat4
            libgdbm-dev
            libgdbm6
            libgettextlib
            libgettextsrc
            libgmp10
            libidn2-0
            libmpc3
            libmpfr6
            libopcodes
            libqt5charts-examples
            libqt5charts-plugins
            libqt5charts-qmlplugins
            libqt5charts5
            libqt5sensors-plugins
            libqt5sensors-qmlplugins
            libqt5sensors5
            libqt5serialport-examples
            libqt5serialport-plugins
            libqt5serialport-qmlplugins
            libqt5serialport5
            libqt5svg-examples
            libqt5svg-plugins
            libqt5svg-qmlplugins
            libqt5svg5
            libqt5virtualkeyboard-plugins
            libqt5virtualkeyboard-qmlplugins
            libqt5virtualkeyboard5
            libqt5webchannel-plugins
            libqt5webchannel-qmlplugins
            libqt5webchannel5
            libreadline-dev
            libreadline8
            libstdc++-dev
            libstdc++6
            libunistring2
            m4-dev
            m4
            make
            nettle
            parted
            piglit
            qt3d-plugins
            qt3d-qmlplugins
            qt3d
            qtbase-examples
            qtbase-plugins
            qtbase-qmlplugins
            qtbase
            qtconnectivity-plugins
            qtconnectivity-qmlplugins
            qtconnectivity
            qtdeclarative-plugins
            qtdeclarative-qmlplugins
            qtdeclarative-tools
            qtdeclarative
            qtgraphicaleffects-qmlplugins
            qtlocation-examples
            qtlocation-plugins
            qtlocation-qmlplugins
            qtlocation
            qtmultimedia-examples
            qtmultimedia-plugins
            qtmultimedia-qmlplugins
            qtmultimedia
            qtquick3d-plugins
            qtquick3d-qmlplugins
            qtquick3d
            qtquics-qmlplugins.control
            qtquics2-plugins.control
            qtquics2-qmlplugins.control
            qtquics2.control
            qtscript-examples
            qtscript-plugins
            qtscript-qmlplugins
            qtscript
            qtwayland-examples
            qtwayland-plugins
            qtwayland-qmlplugins
            qtwayland
            tar
            which
    
    If you do not wish to distribute GPL-3.0 components please remove
    the above packages prior to distribution.  This can be done using
    the opkg remove command.  i.e.:
        opkg remove <package>
    Where <package> is the name printed in the list above
    
    NOTE: If the package is a dependency of another package you
          will be notified of the dependent packages.  You should
          use the --force-removal-of-dependent-packages option to
          also remove the dependent packages as well
    ***************************************************************
    ***************************************************************
    [  OK  ] Finished Print notice about GPLv3 packages.
    [  OK  ] Stopped Weston, a Wayland …mpositor, as a system service.
    [   12.166720] am65-cpsw-nuss 8000000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
    [   12.175416] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [  OK  ] Started EdgeAI OOB demos.
    [  OK  ] Reached target Multi-User System.
    [  OK  ] Reached target Graphical Interface.
             Starting Record Runlevel Change in UTMP...
    [  OK  ] Finished Record Runlevel Change in UTMP.
    
     _____                    _____           _         _
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|
                  |___|                    |___|
    
    Arago Project am62axx-evm -
    
    Arago 2023.10 am62axx-evm -
    
    am62axx-evm login: root
    [   16.990085] audit: type=1006 audit(1651169551.936:10): pid=1235 uid=0 old-auid=4294967295 auid=0 tty=(none) old-ses=4294967295 ses=3 res=1
    [   17.003293] audit: type=1300 audit(1651169551.936:10): arch=c00000b7 syscall=64 success=yes exit=1 a0=8 a1=fffffa93a688 a2=1 a3=ffff895fc020 items=0 ppid=1 pid=1235 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="(systemd)" exe="/lib/systemd/systemd" key=(null)
    [   17.030040] audit: type=1327 audit(1651169551.936:10): proctitle="(systemd)"
    [   17.058707] audit: type=1334 audit(1651169552.004:11): prog-id=11 op=LOAD
    [   17.065684] audit: type=1300 audit(1651169552.004:11): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff6a3a6e0 a2=78 a3=0 items=0 ppid=1 pid=1235 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   17.091285] audit: type=1327 audit(1651169552.004:11): proctitle="(systemd)"
    [   17.098440] audit: type=1334 audit(1651169552.004:12): prog-id=11 op=UNLOAD
    [   17.105471] audit: type=1334 audit(1651169552.004:13): prog-id=12 op=LOAD
    [   17.112363] audit: type=1300 audit(1651169552.004:13): arch=c00000b7 syscall=280 success=yes exit=8 a0=5 a1=fffff6a3a780 a2=78 a3=0 items=0 ppid=1 pid=1235 auid=0 uid=0 gid=0 euid=0 suid=0 fsuid=0 egid=0 sgid=0 fsgid=0 tty=(none) ses=3 comm="systemd" exe="/lib/systemd/systemd" key=(null)
    [   17.137872] audit: type=1327 audit(1651169552.004:13): proctitle="(systemd)"
    

  • I found the problem. I reversed the BOOTMODE switches on SW2 (i.e. the pin order was flipped so switch 1 was set to what 8 should have been set to and so on). I haven't taken the time to look at what mode that was set for but I assume it was something that affected the network. Maybe this will help someone else who accidentally makes the same mistake at least.