This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDA4VH-Q1: The issue of inference with configuration "inDataPadInTIDL"

Part Number: TDA4VH-Q1

There are two models named "35414.tar" and "35447.tar".

We deployed the two models using configuration "inDataPadInTIDL: 1". However there are different issue with the two models.

The model named "35414.tar" will hang in tidl when inferring.

The model named "35447.tar" will get incorrect output.

We have also tried other models with the same configuration and they all work fine. Please help me check what the problem is.

35414.tar35447.tar