This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM5728: Software Reset McASP and EDMA3 modules

Part Number: AM5728

Hello,

I am working with the AM5728 SoC. I am making use of 4 McASP modules and the DSP1-EDMA module in my application. The application runs correctly on device power up or on hardware reset of the entire board. If I just restart the application in CCS, the functionality of the McASP and DSP1-EDMA modules messes up. My application puts the McASP state machines in reset at the beginning by setting the MCASP_GBLCTL register (pg.6139 of TRM) to 0x00000000. However, that doesn't help. 


Is there any other way to reset the McASP and DSP1-EDMA modules thru software so that the application can work well without any hardware reset ?

Thanks,

Dimple