Hi,
I am using the lib (edma3_lld_01_10_00_01). I have a task to optimize copy from External to Internal memory. Say 16K Bytes array. What is your suggestion?
IF this array is contiguous array (1-Dimensional) what should be ACNT, BCNT, CCNT? What is the basis to define these values for a single 1-D array?
And also my results are a bit confusing:
1K~2K Bytes DMA takes more processing cycles than 4K?
And 128 bytes DMA take 6K Cycles?
Why is that L2 to External DMA takes less cycles compared to External memory to L2?
And also Which is the best way to DMA? Is it QDMA? Can QDMA be chained?
-------------------- External Memory to Internal L2 -------------------------
| Bytes | From Setup to DMA completion | From Enable to DMA completion |
| 16K | 51,042 | 24,514 |
| 8K | 45,918 | 10,274 |
| 4K | 43,365 | 7,966 |
| 1K | 34,662 | 8,210 |
| 128 | 30,551 | 5,699 |
| DMA from External L2D to SDRAM | From Enable to DMA completion | |
| Bytes | Clock Cycles from DMA setup to DMA Complete/teardown | |
| 16K | 47,819 | 16,684 |
| 8K | 45,302 | 19,309 |
| 4K | 41,040 | 8,049 |
| 2K | 40,152 | 8,746 |
| 1K | 30,299 | 8,220 |
| 128 | 25,757 | 5,744 |
-------------------- L2 Internal to External Memory -------------------------
unsigned int acnt = MAX_ACOUNT; // Byte Count
unsigned int bcnt = MAX_BCOUNT; // 1
unsigned int ccnt = MAX_CCOUNT; // 1
EDMA3_DRV_SyncType syncType = EDMA3_DRV_SYNC_A;
EDMA3_DRV_Result result = EDMA3_DRV_SOK;
EDMA3_DRV_PaRAMRegs paramSet = {0,0,0,0,0,0,0,0,0,0,0,0};
unsigned int Istestpassed;
unsigned int chId = 0;
unsigned int tcc = 0;
int i;
unsigned int numenabled = 0;
unsigned int BRCnt = 0;
int srcbidx = 0, desbidx = 0;
int srccidx = 0, descidx = 0;
unsigned int *srcuintptr, *dstuintptr;
EDMA3_DRV_Result edmaResult = EDMA3_DRV_SOK;
srcBuff1 = (signed char*)_srcBuff1;
dstBuff1 = (signed char*)_dstBuff1;
/* Initialize EDMA3 first */
edmaResult = edma3init();
for (i = 0; i < (acnt*bcnt*ccnt); i++)
srcBuff1[i] = (char) (i%(0xFF));
BCACHE_wbInvAll(); // 8011 cycles for 8K
BCACHE_inv(srcBuff1, (acnt*bcnt*ccnt), TRUE); // 2811 cycles for 8K
BCACHE_inv(dstBuff1, (acnt*bcnt*ccnt), TRUE); // 2811 cycles for 8K
===================================== MCPS estimate STARTs "From Setup to DMA completion"===================
/* Flush the Source Buffer */
if (result == EDMA3_DRV_SOK)
{
result = Edma3_CacheFlush((unsigned int)srcBuff1, (acnt*bcnt*ccnt));
}
/* Invalidate the Destination Buffer */
if (result == EDMA3_DRV_SOK)
{
result = Edma3_CacheInvalidate((unsigned int)dstBuff1, (acnt*bcnt*ccnt));
}
/* Set B count reload as B count. */
BRCnt = bcnt;
/* Setting up the SRC/DES Index */
srcbidx = (int)acnt;
desbidx = (int)acnt;
if (syncType == EDMA3_DRV_SYNC_A)
{
/* A Sync Transfer Mode */
srccidx = (int)acnt;
descidx = (int)acnt;
}
else
{
/* AB Sync Transfer Mode */
srccidx = ((int)acnt * (int)bcnt);
descidx = ((int)acnt * (int)bcnt);
}
/* Setup for Channel 1*/
tcc = EDMA3_DRV_TCC_ANY;
chId = EDMA3_DRV_DMA_CHANNEL_ANY;
/* Request any DMA channel and any TCC */
if (result == EDMA3_DRV_SOK)
{
result = EDMA3_DRV_requestChannel (hEdma, &chId, &tcc,
(EDMA3_RM_EventQueue)0,
&callback1, NULL);
}
if (result == EDMA3_DRV_SOK)
{
/* Fill the PaRAM Set with transfer specific information */
paramSet.srcAddr = (unsigned int)(srcBuff1);
paramSet.destAddr = (unsigned int)(dstBuff1);
/**
* Be Careful !!!
* Valid values for SRCBIDX/DSTBIDX are between –32768 and 32767
* Valid values for SRCCIDX/DSTCIDX are between –32768 and 32767
*/
paramSet.srcBIdx = srcbidx;
paramSet.destBIdx = desbidx;
paramSet.srcCIdx = srccidx;
paramSet.destCIdx = descidx;
/**
// * Be Careful !!!
* Valid values for ACNT/BCNT/CCNT are between 0 and 65535.
* ACNT/BCNT/CCNT must be greater than or equal to 1.
* Maximum number of bytes in an array (ACNT) is 65535 bytes
* Maximum number of arrays in a frame (BCNT) is 65535
* Maximum number of frames in a block (CCNT) is 65535
*/
paramSet.aCnt = acnt;
paramSet.bCnt = bcnt;
paramSet.cCnt = ccnt;
/* For AB-synchronized transfers, BCNTRLD is not used. */
paramSet.bCntReload = BRCnt;
paramSet.linkAddr = 0xFFFFu;
/* Src & Dest are in INCR modes */
paramSet.opt &= 0xFFFFFFFCu;
/* Program the TCC */
paramSet.opt |= ((tcc << OPT_TCC_SHIFT) & OPT_TCC_MASK);
/* Enable Intermediate & Final transfer completion interrupt */
paramSet.opt |= (1 << OPT_ITCINTEN_SHIFT);
paramSet.opt |= (1 << OPT_TCINTEN_SHIFT);
if (syncType == EDMA3_DRV_SYNC_A)
{
paramSet.opt &= 0xFFFFFFFBu;
}
else
{
/* AB Sync Transfer Mode */
paramSet.opt |= (1 << OPT_SYNCDIM_SHIFT);
}
/* Now, write the PaRAM Set. */
result = EDMA3_DRV_setPaRAM(hEdma, chId, ¶mSet);
}
/*
* Since the transfer is going to happen in Manual mode of EDMA3
* operation, we have to 'Enable the Transfer' multiple times.
* Number of times depends upon the Mode (A/AB Sync)
* and the different counts.
*/
if (result == EDMA3_DRV_SOK)
{
/*Need to activate next param*/
if (syncType == EDMA3_DRV_SYNC_A)
{
numenabled = bcnt * ccnt;
}
else
{
/* AB Sync Transfer Mode */
numenabled = ccnt;
}
for (i = 0; i < numenabled; i++)
{
irqRaised1 = 0;
===================================== MCPS estimate STARTs "From Enable to DMA completion"===================
/*
* Now enable the transfer as many times as calculated above.
*/
result = EDMA3_DRV_enableTransfer (hEdma, chId, //EDMA3_DRV_TRIG_MODE_NONE);
EDMA3_DRV_TRIG_MODE_MANUAL);
if (result != EDMA3_DRV_SOK)
{
printf ("edma3_test: EDMA3_DRV_enableTransfer " \
"Failed, error code: %d\r\n", result);
break;
}
/* Wait for the Completion ISR. */
while (irqRaised1 == 0u)
{
/** Wait for the Completion ISR on Master Channel.
* You can insert your code here to do something
* meaningful.
*/
}
/* Check the status of the completed transfer */
if (irqRaised1 < 0)
{
/* Some error occured, break from the FOR loop. */
printf ("\r\nedma3_test: Event Miss Occured!!!\r\n");
/* Clear the error bits first */
result = EDMA3_DRV_clearErrorBits (hEdma, chId);
break;
}
===================================== MCPS estimate END ===================
}
}
/* Match the Source and Destination Buffers. */
if (EDMA3_DRV_SOK == result)
{
/* Free the previously allocated channel. */
result = EDMA3_DRV_freeChannel (hEdma, chId);
if (result != EDMA3_DRV_SOK)
{
printf("edma3_test: EDMA3_DRV_freeChannel() FAILED, " \
"error code: %d\r\n", result);
}
}
}