Part Number: SK-AM62A-LP
Hello,
We're currently attempting to run vision_apps demos on SITARA for QNX but we've ran into an issue - the IPC does not get initialised, resulting in hangs on graph verification (IPC between MPU and MCU1_0 fails).
Comparing our log with the log from docs, we notice that the IPC never gets to "Done" state, while in TI's logs "IPC: Waiting for HLOS to be ready ... !!!" is never printed out.
Our current log is:
[MCU1_0] 0.041292 s: APP: Init ... !!!
[MCU1_0] 0.041327 s: MEM: Init ... !!!
[MCU1_0] 0.041348 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ af000000 of size 16777216 bytes !!!
[MCU1_0] 0.041401 s: MEM: Init ... Done !!!
[MCU1_0] 0.041419 s: IPC: Init ... !!!
[MCU1_0] 0.041438 s: IPC: 3 CPUs participating in IPC !!!
[MCU1_0] 0.041751 s: IPC: Waiting for HLOS to be ready ... !!!
[MCU1_0] 0.046241 s: #Sciserver Version: v2023.06.0.0-REL.MCUSDK.09.00.00.14+
[MCU1_0] 0.049014 s: ##RM_PM_HAL Version: v09.00.05
[MCU1_0] 0.051961 s: ##Starting Sciserver..... PASSED
The log in the documentation is:
[MCU1_0] 1.113785 s: CIO: Init ... Done !!!
[MCU1_0] 1.113841 s: ### CPU Frequency = 800000000 Hz
[MCU1_0] 1.113864 s: APP: Init ... !!!
[MCU1_0] 1.113877 s: MEM: Init ... !!!
[MCU1_0] 1.113895 s: MEM: Created heap (DDR_LOCAL_MEM, id=0, flags=0x00000004) @ af000000 of size 16777216 bytes !!!
[MCU1_0] 1.113946 s: MEM: Init ... Done !!!
[MCU1_0] 1.113962 s: IPC: Init ... !!!
[MCU1_0] 1.113999 s: IPC: 3 CPUs participating in IPC !!!
[MCU1_0] 1.115241 s: IPC: Init ... Done !!!
[MCU1_0] 1.115269 s: APP: Syncing with 2 CPUs ... !!!
[MCU1_0] 1.115291 s: APP: Syncing with 2 CPUs ... Done !!!
[MCU1_0] 1.115328 s: REMOTE_SERVICE: Init ... !!!
[MCU1_0] 1.115826 s: REMOTE_SERVICE: Init ... Done !!!
[MCU1_0] 1.115855 s: FVID2: Init ... !!!
[MCU1_0] 1.115885 s: FVID2: Init ... Done !!!
[MCU1_0] 1.115902 s: VHWA: VPAC Init ... !!!
[MCU1_0] 1.115917 s: SCICLIENT: Sciclient_pmSetModuleState module=219 state=2
[MCU1_0] 1.116065 s: SCICLIENT: Sciclient_pmSetModuleState success
[MCU1_0] 1.116097 s: VHWA: LDC Init ... !!!
[MCU1_0] 1.116344 s: VHWA: LDC Init ... Done !!!
[MCU1_0] 1.116431 s: VHWA: MSC Init ... !!!
[MCU1_0] 1.117080 s: VHWA: MSC Init ... Done !!!
[MCU1_0] 1.117103 s: VHWA: VISS Init ... !!!
[MCU1_0] 1.117389 s: VHWA: VISS Init ... Done !!!
[MCU1_0] 1.117414 s: VHWA: VPAC Init ... Done !!!
[MCU1_0] 1.117492 s: VX_ZONE_INIT:Enabled
[MCU1_0] 1.117514 s: VX_ZONE_ERROR:Enabled
[MCU1_0] 1.117532 s: VX_ZONE_WARNING:Enabled
[MCU1_0] 1.118205 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target MCU1-0
[MCU1_0] 1.118314 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_LDC1
[MCU1_0] 1.118405 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC1
[MCU1_0] 1.118499 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_MSC2
[MCU1_0] 1.118600 s: VX_ZONE_INIT:[tivxPlatformCreateTargetId:66] Added target VPAC_VISS1
[MCU1_0] 1.118632 s: VX_ZONE_INIT:[tivxInitLocal:130] Initialization Done !!!
[MCU1_0] 1.118653 s: APP: OpenVX Target kernel init ... !!!
[MCU1_0] 1.122696 s: APP: OpenVX Target kernel init ... Done !!!
[MCU1_0] 1.122723 s: VISS REMOTE SERVICE: Init ... !!!
[MCU1_0] 1.122769 s: VISS REMOTE SERVICE: Init ... Done !!!
[MCU1_0] 1.122812 s: APP: Init ... Done !!!
[MCU1_0] 1.122830 s: APP: Run ... !!!
[MCU1_0] 1.122843 s: IPC: Starting echo test ...
[MCU1_0] 1.123376 s: APP: Run ... Done !!!
[MCU1_0] 1.123485 s: IPC: Echo status: mpu1_0[x] mcu1_0[s] c7x_1[P]
We suspect this behaviour is caused by the tiboot3.bin file we're using - it's the prebuilt tiboot3.bin that comes with the SDK.
The SDK we're using is ti-processor-sdk-qnx_am62axx_09_00_00_01.
Thank you for your time!
Best regards
Hristo