Part Number: AM69
・The current CPU (LS1046A NXP) is 64 bit x 1, but the AM69 series is 32 bit x 4. Will this be degraded compared to the current memory bandwidth?
If we can think of 32-bit x4=128-bit, it seems like an upgrade, but I think so. Also, I would like to know why the memory bus is 32-bit, even though it is a 64-bit core.
・Could you tell me the power consumption for AM69 at the use rate below?
-AM69 (A72x4)
50%:
60%:
70%:
80%:
90%:
100%:
-AM69 (A72x8)
50%:
60%:
70%:
80%:
90%:
100%: