Other Parts Discussed in Thread: SYSBIOS
Hello,
After compiling and flashing the Linux + SYSBIOS w/Syslink demo onto my EVM6678L demo board my system will not mount the root file system. I get the following printout at the serial console:
Designed for the EVMC6678 board, Texas Instruments.
CPU0: C66x rev 0x0, 1.2 volts, 1000MHz
Initializing kernel
Built 1 zonelists in Zone order, mobility grouping on. Total pages: 130048
Kernel command line: console=ttyS0,115200 initrd=0x80400000,0x1700000 ip=dhcp rw
PID hash table entries: 2048 (order: 1, 8192 bytes)
Dentry cache hash table entries: 65536 (order: 6, 262144 bytes)
Inode-cache hash table entries: 32768 (order: 5, 131072 bytes)
Memory available: 492256k/520316k RAM, 0k/0k ROM (788k kernel code, 202k data)
SLUB: Genslabs=7, HWalign=128, Order=0-3, MinObjects=0, CPUs=1, Nodes=1
Hierarchical RCU implementation.
RCU-based detection of stalled CPUs is enabled.
NR_IRQS:288
Console: colour dummy device 80x25
Calibrating delay loop... 999.42 BogoMIPS (lpj=1998848)
Mount-cache hash table entries: 512
C64x: 9 gpio irqs
NET: Registered protocol family 16
SGMII init complete
bio: create slab <bio-0> at 0
Switching to clocksource TSC64
NET: Registered protocol family 2
IP route cache hash table entries: 4096 (order: 2, 16384 bytes)
TCP established hash table entries: 16384 (order: 5, 131072 bytes)
TCP bind hash table entries: 16384 (order: 4, 65536 bytes)
TCP: Hash tables configured (established 16384 bind 16384)
TCP reno registered
UDP hash table entries: 256 (order: 0, 4096 bytes)
UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
NET: Registered protocol family 1
RPC: Registered udp transport module.
RPC: Registered tcp transport module.
RPC: Registered tcp NFSv4.1 backchannel transport module.
Trying to unpack rootfs image as initramfs...
rootfs image is not initramfs (junk in compressed archive); looks like an initrd
Freeing initrd memory: 23552k freed
JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
ROMFS MTD (C) 2007 Red Hat, Inc.
msgmni has been set to 1007
Block layer SCSI generic (bsg) driver version 0.4 loaded (major 254)
io scheduler noop registered
io scheduler deadline registered
io scheduler cfq registered (default)
Serial: 8250/16550 driver, 1 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO 0x2540000 (irq = 276) is a 16550A
console [ttyS0] enabled
brd: module loaded
loop: module loaded
at24 1-0050: 131072 byte 24c1024 EEPROM (writable)
uclinux[mtd]: RAM probe address=0x803e0760 size=0x0
Creating 1 MTD partitions on "RAM":
0x000000000000-0x000000000000 : "ROMfs"
mtd: partition "ROMfs" is out of reach -- disabled
Generic platform RAM MTD, (c) 2004 Simtec Electronics
NAND device: Manufacturer ID: 0x20, Chip ID: 0x36 (ST Micro NAND 64MiB 1,8V 8-b)
Scanning device for bad blocks
Creating 3 MTD partitions on "davinci_nand.0":
0x000000000000-0x000000004000 : "bootconfig"
0x000000004000-0x000001000000 : "kernel"
0x000001000000-0x000004000000 : "filesystem"
davinci_nand davinci_nand.0: controller rev. 2.5
m25p80 spi0.0: n25q128 (16384 Kbytes)
Creating 1 MTD partitions on "spi_flash":
0x000000000000-0x000001000000 : "test"
spi_davinci spi_davinci.0: Controller at 0x20bf0000
spi_davinci spi_davinci.0: Operating in interrupt mode using IRQ 182
keystone_netcp keystone_netcp.0: firmware: using built-in firmware keystone-pdsw
keystone_netcp keystone_netcp.0: firmware: using built-in firmware keystone-pdsw
pktgen 2.72: Packet Generator for packet performance testing.
TCP cubic registered
NET: Registered protocol family 17
Sending DHCP requests .., OK
IP-Config: Got DHCP answer from 192.168.1.1, my address is 192.168.1.107
IP-Config: Complete:
device=eth0, addr=192.168.1.107, mask=255.255.255.0, gw=192.168.1.1,
host=192.168.1.107, domain=hsd1.ca.comcast.net., nis-domain=(none),
bootserver=192.168.1.1, rootserver=192.168.1.1, rootpath=
RAMDISK: gzip image found at block 0
RAMDISK: incomplete write (28179 != 32768)
write error
Looking up port of RPC 100003/2 on 192.168.1.1
rpcbind: server 192.168.1.1 not responding, timed out
Root-NFS: Unable to get nfsd port number from server, using default
Looking up port of RPC 100005/1 on 192.168.1.1
rpcbind: server 192.168.1.1 not responding, timed out
Root-NFS: Unable to get mountd port number from server, using default
Root-NFS: Server returned error -110 while mounting /tftpboot/192.168.1.107
VFS: Unable to mount root fs via NFS, trying floppy.
VFS: Cannot open root device "(null)" or unknown-block(2,0)
Please append a correct "root=" boot option; here are the available partitions:
1f01 16 mtdblock1 (driver?)
1f02 16368 mtdblock2 (driver?)
1f03 49152 mtdblock3 (driver?)
1f04 16384 mtdblock4 (driver?)
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)
Stack from 9e017f2c:
803130a4 803130a8 80339efb 803c53e8 00000000 9e00a012 9e00a000 803a0134
80337faf 9e017f60 9e017f60 00000000 73020002 6e6b6e75 2d6e776f 636f6c62
2c32286b 00002930 00000000 00000000 8031317c 00000080 00000000 00000000
803a0648 803c3240 803bfd48 00000000 00000000 00000000 00000000 00000000
00000000 00000000 00000000 00000000 803c1ba4 803c1ba4 00000000 803c1ba4
803c1ba4 8039fb48 00000000 00000000 00000000 00000000 00000000 80001e6c
Call trace: [<803130a4>] panic+0x64/0x120
[<803130a8>] panic+0x68/0x120
[<803a0134>] mount_block_root+0x2e8/0x30c
[<8031317c>] printk+0x1c/0x40
[<803a0648>] prepare_namespace+0x234/0x28c
[<8039fb48>] kernel_init+0x1c4/0x1fc
[<80001e6c>] kernel_thread_helper+0x18/0x1c
INFO: RCU detected CPU 0 stall (t=2500 jiffies)
INFO: RCU detected CPU 0 stall (t=10000 jiffies)
INFO: RCU detected CPU 0 stall (t=17500 jiffies)
INFO: RCU detected CPU 0 stall (t=25000 jiffies)
INFO: RCU detected CPU 0 stall (t=32500 jiffies)