This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C5515 SPI flash boot

Other Parts Discussed in Thread: TMS320C5515

Can someone confirm that I am able to boot the TMS320C5515 from a S70FL256P (256-Mbit CMOS 3.0 Volt Flash Memory) as long as I connect it to CS0? Anyone have any suggestions?  According to the following it looks like I'm OK.

 

Please see our C5505 bootloader appnote, Using the TMS320C5505/04 Bootloader:

 

“The bootloader supports booting from an SPI EEPROM with the following requirements for the external

device:

• The device must support at least a 500 kHz SPI clock.

• The device must be connected to SPI CS0 and act as an SPI slave.

• The device uses 2 bytes (16 bits) for internal addressing (up to 64kB).

• The device must have the capability to auto-increment its internal address counter to allow sequential reads from the device.

• The device can be connected to either valid pin-mapping for SPI; there are two distinct pin-mappings available. The bootloader attempts to communicate on each SPI pin-mapping, one at a time."

 

The SPI EEPROM should support 16-bit addressing and 8-bit data.

 

Victor