This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Memory Bank

I know Memory Bank can stall the pipeline, so we should avoid it.

Question1:

As the description of TI's datasheet, it won't stall the pipeline, if  we access the same bank that in deferent "Block" or say "Memory Space". My question is that :

1)How to obtain the information about "Block" or "Memory Space"?

2)Can I configure my memory into deferent "Block" or "Memory Space" through some directive?

 

Question2:

There are 4 Banks(Bank0, Bank1, Bank2, Bank3) in each memory space, and 2 bytes per bank  for C6000 devices as datasheet of "TMS320C6000 Optimizing Compiler v7.0 User's Guide"(SPRU187Q, 4.5 Avoiding Memory Bank Conflicts With the Assembly Optimizer ).

But I found a contradiction from "4.2.1.3 L2 Memory Banking" in datasheet of "TMS320C64x+ DSP Megamodule Reference Guide"(SPRU871K). It's description about L2 Memory Banking is defferent from SPRU425A. details as followings:

The L2 memory implements two separate memory ports. Each memory port can control one of:
• 4 × 128-bit banks
• 2 × 128-bit banks
• 1 × 256-bit bank
Refer to the device-specific data manual for more information about the banking scheme implemented on a particular device.
The two memory ports may address memory sections which may or may not be contiguous.

I want to know how to understand the defferences between the two datasheet

Is there anyone would give me some promption, or some references document ?