This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

rtdxx.lib for C2000 source

 Hello,

I have an issue with rtdxx.lib for C2000 described in a post named "Simulink to F28335 communication using RTDX" on "TMS320C2000™ 32-bit Real-time MCUs" forum (http://e2e.ti.com/support/microcontrollers/tms320c2000_32-bit_real-time_mcus/f/171/t/130663.aspx). Here I will only repeat my questions to which I didn't get answers on the aforementioned forum:

  1. Is it possible to obtain a project from which rtdxx.lib in DSP/BIOS 5.31.x was built so I can rebuild it for F28335 with FPU support?
  2. Is there a way to make rtdxx.lib (DSP/BIOS 5.31.x) link into a F28335 CCS project with FPU support?

Thanks in advance!