Other Parts Discussed in Thread: TMS320VC5416, CCSTUDIO
Hi friends,
I'm using TMS320VC5416 communicating with Atmega128 via HPI interface. I want to use Atmega to boot-up DSP via HPI interface at enhanced 8 bit HPI mode.
The application (for DSP) is organized in 3 sections: 80h (DARAM), 28000h(SARAM), 38000h(SARAM). Throughout HPI, I can write and read at the DARAM (80h), but I can not write at 28000h and 38000h. Anybody can help me to guess the cause of the failure? Does DSP need any special configurations?
Any help is highly appreciated
Thanks in advanced
TungDH