This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM3352: Json-C library vulnerablity in dunfell yocto

Part Number: AM3352

Hi All,

Can we utilize the JSON-C library versions 0.17 or 0.16 with TiSDK 18.04?

as we are seeing the vulnerabilities in json-c 0.13.1 version so we want to upgrade the version 0.16 or 0.17.

We have tried to replace 0.13.1 to 0.17 and at the time of compile/build we faced the below error,

ERROR: core-app-1.0-r0 do_package_qa: QA Issue: /usr/sem3/bin/core-app contained in package core-app requires libjson-c.so.4, but no providers found in RDEPENDS_core-app? [file-rdeps]
ERROR: core-app-1.0-r0 do_package_qa: QA run found fatal errors. Please consider fixing them.
ERROR: Logfile of failure stored in: /home/sem3user2/1.3.0.AB_Latest/SEM3T_COM/build/arago-tmp-external-arm-glibc/work/armv7at2hf-neon-linux-gnueabi/core-app/1.0-r0/temp/log.do_package_qa.70035
ERROR: Task (/home/sem3user2/1.3.0.AB_Latest/SEM3T_COM/sources/meta-sem3t/recipes-core/app/core-app.bb:do_package_qa) failed with exit code '1'
NOTE: Tasks Summary: Attempted 3556 tasks of which 3549 didn't need to be rerun and 1 failed.
NOTE: Writing buildhistory
NOTE: Writing buildhistory took: 3 seconds

Is it possible to upgrade json-c version in tisdk 18.04 or not.

.

Please clariffy

Background: