Regarding the H264 and MPEG2 codecs for the DM8168:
1) Where can I obtain datasheets for these codecs? There is no information at all in the "omx" directory of EZSDK 5.02.01.59 that I am using at present.
2) What resources do these codecs use?
3) How can I configure the resources that are used?
4) Is all control for these codecs done by the Media Controller?
5) Is the DSP used at all by these codecs?
Thanks,
Ralph