This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168 H264 and MPEG2 Codecs

Guru 10685 points

Regarding the H264 and MPEG2 codecs for the DM8168:

1) Where can I obtain datasheets for these codecs? There is no information at all in the "omx" directory of EZSDK 5.02.01.59 that I am using at present.

2) What resources do these codecs use?

3) How can I configure the resources that are used?

4) Is all control for these codecs done by the Media Controller?

5) Is the DSP used at all by these codecs?

Thanks,
Ralph