This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J7200XSOMXEVM: ROM code boottime when sd card is set as primary boot

Part Number: J7200XSOMXEVM

Hi all,

We've configured the evm board to use the SD card as the primary boot and eMMC as the secondary boot. This works pretty much as expected, but if there is no SD card inserted or a blank SD card is inserted the ROM seems to take about 10s before booting from the eMMC. Could this be configured to run faster? Reversing the configuration, i.e. setting eMMC as primary and SD card as secondary, the ROM will boot from SD card near instantly, when we've wiped the eMMC.

-Juha