Part Number: EVMK2GX
Hi all,
I have few questions regarding K2G eval board.
I am using Evaluation board : EVMK2GX to work with it, I downloaded ti-processor-sdk-linux-k2g-evm-06.03.00.106-Linux-x86-Install.bin
Below are the different approach, I had taken to generate MLO, u-boot images.
- Executed the create-sdcard.sh part of bin folder, it would load pre build tarball and u-boot binaries.
- Secondly move to makefile which is part of main folder in downloaded sdk and executed u-boot-spl_clean, u-boot-spl
- Also, manually ran below commands to compile u-boot
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- distclean
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf- k2g_evm_defconfig
make ARCH=arm CROSS_COMPILE=arm-linux-gnueabihf-
In all above cases final outcome was same as below, it seems u-boot is stuck at DRAM
U-Boot 2019.01-gb9a02a7d56-dirty (Jan 30 2024 - 11:04:22 -0500)
CPU: 66AK2Gx-100 SR1.0
Model: Texas Instruments K2G General Purpose EVM
DRAM:
Thanks,
Chintan Gala