This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM68: AM68

Part Number: AM68


Dear TI,

for a new design I need a ARM based processor plus VPU and GPU.

The main requirements are related to the video output format that I have to implement.

Final product must be configurable in 3 different ways:

1. Manage two independent Panels, FHD, 1080p, or

2. Manage one Panel, 4Kp60 with EDP interface, or

3. Manage one Panel, 4Kp60 with V-by-One interface

VPU:

1. H265 HEVC profiles MP/MP10 @ 4K/60fps
2. VP9 @ 4K/60fps
3. H264 AVC profiles BP/MP/XP/HP @ 1080P/30fps
4. MPEG-4 profiles SP/ASP @ 720P/30fps

GPU: OpenGL ES 2.0.

 Which could be a TI processor able to manage these configurations? 

Thank you

Best Regards

Corrado