Dear all,
Where can I obtain test application that is media-control Framework aware or compatible to stream from MT9V032 camera sensor and output to the LCD touchscreen display?
Previously, I can do "export DISPLAY=:0.0" and "gst-launch v4l2 ! xvimagesink" to get the camera stream to display on the LCD using 2.6.34.
But with MC-framework in newer kernel, what test application can I use to do the same to display the camera output to LCD screen?
Many thanks in adv.
James