Part Number: AM625
Other Parts Discussed in Thread: SK-AM62, SK-AM62-LP, TPS65219, SK-AM62B-P1
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: AM625
Other Parts Discussed in Thread: SK-AM62, SK-AM62-LP, TPS65219, SK-AM62B-P1
Hello Hemal Patel
Thank you for the query.
I saw a similar query where is suggested to split the questions.
For Q.2 i will assign to the PMIC team and will request them to assign to the POE team.
Regards,
Sreenivasa
Hi,
Is this for an automotive or non-automotive application? We have multiple TPS65219 part numbers that are pre-configured to support different application requirements and use cases. TPS6521920 supports automotive applications using AM62x-Q1 (17x17mm AMC package), VDD_CORE=0.75V and LPDDR4. Below are the PMIC resources that are available. Let us know if there are any questions.
Thanks,
Brenda
Hii,
Thanks for the response.
Our application is non-automotive and TPS6521903 (non-automotive applications, VDD_CORE=0.75V, DDR4) seems more suitable for application so we are considering this part in our design.
> We request you to provide POE [12W] & DC [12V & 1A] based power supply ref. schematic
Hi,
I'm not sure if I understand the request in your previous message. The design files from the AM62 starter kit is what we have available to assist the design process for applications using the TPS65219 PMIC to power the AM62 processor.
Are you looking for a pre-regulator to convert from 12V to 5V or 3.3V?
Thanks,
Brenda