HI,
i am working on DM368-IPNC reference design but i am facing some issues:
1.I have made by own uimage and cramfs image but i am not able to boot the board using my images.
The board boots fine when uimage and cramfs that come with the package are installed.
The boot process is getting stuck before the login prompt .
Also when i am trying to mount the filesystem on the board using nfs using the userguide section 2.4.4
2.4.4 Booting from Flash Using NFS File System
i am getting the following output.
IP-Config: No network devices available.                                        
Looking up port of RPC 100003/2 on 10.17.8.125                                  
portmap: RPC call returned error 101                                            
Root-NFS: Unable to get nfsd port number from server, using default             
Looking up port of RPC 100005/1 on 10.17.8.125                                  
portmap: RPC call returned error 101                                            
Root-NFS: Unable to get mountd port number from server, using default           
mount: RPC call returned error 101                                              
Root-NFS: Server returned error -101 while mounting /home/mayank/DM36x/ipnc/tars
VFS: Unable to mount root fs via NFS, trying floppy.                            
VFS: Cannot open root device "nfs" or unknown-block(2,0)                        
Please append a correct "root=" boot option                                     
Kernel panic - not syncing: VFS: Unable to mount root fs on unknown-block(2,0)  
It is highly unfortunate that steps given in user guide are totally incomplete and they don't
discuss the issues which developers can face while implementing the steps.
Even after trying for several days i am not able to install my own uimage and cramfs imagems on DM368
on DM368 board and boot the board properly and run the algorithms.
If anyone has faced similar problem in the past he can help me.
Is there any other method(other than building own cramfs and installing it on the board and mounting filesystem through nfs)
to execute any of the code or any algorithms on DM368 Board.
Thanks and Regards,
Mayank