DM8148 TRM says that for booting from SD it should be connected to MMC/SD interface #1. I want to double check if this is SD0 interface (table 3-27 in DM8148) datasheet or SD1 interface (table 3-28 in DM8148 datasheet)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
DM8148 TRM says that for booting from SD it should be connected to MMC/SD interface #1. I want to double check if this is SD0 interface (table 3-27 in DM8148) datasheet or SD1 interface (table 3-28 in DM8148 datasheet)?
Manoj,
DM8148 has 3 MMC instances. Booting is supported from 2nd MMC instance, i.e. SD1, which corresponds to Table 3-28 in the DS. You can verify the same from the EVM schematics as well.
Let me know if this clarifies your doubt.