This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SDRAM Window0 Start Address



Hi,

I am working on a DM6446.

I am trying to get a picture I loaded in DDR2 (address 0x80200000) to be displayed in Window0. I have tried loading BMP and YUV422 format files ito DDR2, but the Window0 contents still does not display anything, only a green screen.

How do I specify the start address?

Is VIDWIN0ADR the start address where the picture is loaded?

Is this an offset value or is it the 0x80200000 value?

also, I do not understand how the 5 least significant bits need to be zero.

 

What other settings do I need?

Is there anything that I need to set up specifically for the VPBE to access the DDR2?

 

I am out of ideas, please assist.

Thanks,

Herman van Wyk