This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Error when compiling DVSDK 4.02 for DM365

I was trying to recompile the DVSDK 4.02 for DM365 and got an error. These were my steps:

1) installed CodeSourcery Tools and set the $PATH variable

2)Installed DVSDK from http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/dvsdk/DVSDK_4_00/latest/index_FDS.html
executing ./setup.shdvsdk_dm365-evm_4_02_00_06_setuplinux 

3) Setup DVSDK by executing
ti-dvsdk_dm365-evm_4_02_00_06/setup.sh 

3) cd /ti-dvsdk_dm365-evm_4_02_00_06/psp/linux-2.6.32.17-psp03.01.01.39

4) Cleaned my installation of previous build settings
host$ make distclean ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-

5) Configured the kernel according to the default configuration provided for DM365
host$ make davinci_dm365_defconfig ARCH=arm CROSS_COMPILE=arm-none-linux-gnueabi-

6) make clean

7) make all

Got error: 

pedro@ubuntu:~/ti-dvsdk_dm365-evm_4_02_00_06/psp/linux-2.6.32.17-psp03.01.01.39$ make all

  CHK     include/linux/version.h

make[1]: `include/asm-arm/mach-types.h' is up to date.

  CHK     include/linux/utsrelease.h

  SYMLINK include/asm -> include/asm-arm

  CC      kernel/bounds.s

cc1: error: unrecognized command line option "-mlittle-endian"

cc1: error: unrecognized command line option "-mapcs"

cc1: error: unrecognized command line option "-mno-sched-prolog"

cc1: error: unrecognized command line option "-mabi=aapcs-linux"

cc1: error: unrecognized command line option "-mno-thumb-interwork"

kernel/bounds.c:1: error: bad value (armv4t) for -march= switch

kernel/bounds.c:1: error: bad value (arm9tdmi) for -mtune= switch

make[1]: *** [kernel/bounds.s] Error 1

make: *** [prepare0] Error 2

What's causing this error?