Dear Team,
I hope this message finds you well. I am writing to request verification of the maximum achievable baud rate and data transfer speed for the UART in the AM335x processor.
Specifically, I would like to test the UART at a higher baud rate of 115200 and ascertain its capability to achieve a data transfer speed of 10Mbps.
Could you kindly provide guidance or documentation regarding this matter? Additionally, if there are any specific procedures or test methods recommended for validating these parameters, I would appreciate receiving detailed instructions.
Please feel free to reach out if further clarification or information is required
Thanks & Regards
Lokesh A