This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM625SIP: AM625 Mass Storage Class Feature

Part Number: AM625SIP
Other Parts Discussed in Thread: AM625,

Hello.

Does the AM625 USB support Mass Storage Class?
I want to connect an AM625 to a host and use it as a USB memory.

The AM335x USB was available as shown in the link below.
software-dl.ti.com/.../MUSB.html

I would appreciate your confirmation.
Thank you.

  • Hi Hochun,

    Yes, Linux running on AM625SIP supports Mass Storage Class gadget too. You will need to load the same g_mass_storage.ko module with proper parameters, as long as the the USB port is designed as peripheral mode or DRD mode on the board.