This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PROCESSOR-SDK-AM57X: Gstreamer command does not work well if update SDK version

Genius 3186 points
Part Number: PROCESSOR-SDK-AM57X


Hi

May I have question about processor SDK linux for AM57x?

My customer is using old version SDK for use OpenCV.

And now, updateing SDK 05.03.00.07 to 06.03.00.106.

But there are issues about Gstreamer.

If operate same command in each version, ver 05.03 is works nomally, but ver 06.03 is not work well.

command : gst-launch-1.0 v4l2src

Question 1

Is there anything to difference of Gstreamer each SDK version?

Question 2

Is there difference use way of Gstreamer command option in each SDK version?

Thanks,

GR