Part Number: PROCESSOR-SDK-AM64X
Hi,
I used to see 4 COM Ports 13,14,15,16. (If memory serves me right)
I did the UART load, CCS Hello World Debug, I preformed the DFU load. I am still working on the SD Card Load, etc.
Somewhere along the way I lost 2 Serial Ports, because I went back to the UART load.
Now, I only see 2 Serial Ports: COM 4 and COM 6.
I'm not sure what happened. Maybe I over-wrote something?
Plugging/Unplugging the JTAG has no effect.
Plugging/Unplugging UART port just removes and restores the same 2 USB Serial Ports.
I've tried varying the Boot Switch positions, to no avail.
I searched and found this
e2e.ti.com/.../processor-sdk-am64x-serial-port-not-functioning-properly-can-only-see-2-com-ports
I think they were having the same issue, but there is no answer,
I highly doubt the SDK is broke. I just don't know how to get it back.
Thanks,