cc: Andreas Dannenberg's Profile - Andreas Dannenberg - TI E2E support forums and Nick Saulnier's Profile - Nick Saulnier - TI E2E support forums
I just saw a post TMDS64GPEVM: CCS Studio v11 Linux USB XDS problems - Processors forum - Processors - TI E2E support forums
from 2 years ago insinuating that one cannot run a Linux ( VMWare Workstation) VM installation (with the Linux version of CCS) on a Windows PC and expect 2 USB (virtual) ports to be able to connect into an EVM 2 micro-B ports (one for UART, one for XDS110 on the EVM) and be able to download Linux CCS compiles and debug over CCS?
Is this true? Do I need a PC that is a pure Linux only build to connect up to any EVM for any Linux compiled application?
This might be a root cause scenario for what I am seeing on e2e entry (1) TMDS64EVM: CCS v12.6 Linux cannot tell that if EVM's XDS110 probe "firmware update is required for the XDS110 probe." - Processors forum - Processors - TI E2E support forums that is assigned to (2) Tushar Thakur's Profile - Tushar Thakur - TI E2E support forums
thanks!