This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDVPSS demo does not work on TI816X VS2 daughter card [UNKNOWN BOARD]

Hi all,

I'm working with  TI816X VS2 daughter card

The SDK version is 05_00_00_09.

I run the demo /home/user/ti-ezsdk_dm816x-evm_5_00_00_09/hdvpss_01_00_01_25/build/bin/ti816x-evm/m3vpss/whole_program_debug
hdvpss_examples_chains.xem3 by using CCS4.2

When run the demo there's error occured. 

 The message listed below:

-------------------------------------------------------

[CortexM3_ISS_0]  0: SYSTEM  : System Init in progress !!!

[CortexM3_ISS_0] === HDVPSS Clocks are enabled ===

[CortexM3_ISS_0] === HDVPSS is fully functional ===

[CortexM3_ISS_0] === HDVPSS module is not in standby ===

[CortexM3_ISS_0] === I2C1 Clk is active ===

[CortexM3_ISS_0]  14: SYSTEM : HDVPSS Drivers Version String: HDVPSS_01_00_01_25

[CortexM3_ISS_0] *** VPDMA Firmware Loading... ***

[CortexM3_ISS_0] VPDMA Firmware Address = 0x9234d660

[CortexM3_ISS_0] VPDMA Load Address     = 0x4810d004

[CortexM3_ISS_0] VPDMA Firmware Version = 0x4d000185

[CortexM3_ISS_0] VPDMA List Busy Status = 0x00000000

[CortexM3_ISS_0] *** VPDMA Firmware Load Success ***

[CortexM3_ISS_0] 

[CortexM3_ISS_0]  I2C1: Passed for address 0x20 !!! 

[CortexM3_ISS_0]  I2C1: Passed for address 0x21 !!! 

[CortexM3_ISS_0]  I2C1: Passed for address 0x39 !!! 

[CortexM3_ISS_0]  I2C1: Passed for address 0x3d !!! 

[CortexM3_ISS_0]  I2C1: Passed for address 0x60 !!! 

[CortexM3_ISS_0]  2760: SYSTEM  : System Init Done !!!

[CortexM3_ISS_0]  2760: CHAINS  : Initializing Links !!! 

[CortexM3_ISS_0]  2760: SYSTEM  : Heap Free Space (System = 62512 bytes, Buffer = 220200960 bytes, Mbx = 10240 msgs) 

[CortexM3_ISS_0]  4330: CHAINS  : Initializing Links ... DONE !!! 

[CortexM3_ISS_0]  4330: CHAINS  : CPU Revision [ES1.1] !!! 

[CortexM3_ISS_0]  4330: CHAINS  : Detected [UNKNOWN] Board !!! 

[CortexM3_ISS_0]  4341: CHAINS  : Base Board Revision [REV B] !!! 

[CortexM3_ISS_0] 

[CortexM3_ISS_0]  ============

[CortexM3_ISS_0]  Chain Select

[CortexM3_ISS_0]  ============

[CortexM3_ISS_0] 

[CortexM3_ISS_0]  Current System Settings,

[CortexM3_ISS_0]  Num Video Ports       : 4

[CortexM3_ISS_0]  Number of Displays    : 1

[CortexM3_ISS_0]  Display 1             : HDMI_OFFCHIP

[CortexM3_ISS_0]  Display 2             : HDMI_ONCHIP

[CortexM3_ISS_0]  DEI                   : DEI-HQ

[CortexM3_ISS_0]  DEI Output to Display : DEI-SC

[CortexM3_ISS_0]  NSF Mode              : SNF + TNF

[CortexM3_ISS_0]  Execution Time        : 60 secs

[CortexM3_ISS_0]  Loop Count            : 1

[CortexM3_ISS_0]  GRPX                  : ON

[CortexM3_ISS_0]  Display Resolution    : 1080P60

[CortexM3_ISS_0]  Tiler                 : OFF

[CortexM3_ISS_0]  DEI Compression       : OFF

[CortexM3_ISS_0]  Number of Sub Chains  : 1

[CortexM3_ISS_0]  [UNKNOWN BOARD] 

[CortexM3_ISS_0] 

                                                      stop  here

Does anybody have the same problem?

 

Thanks in advance for any help!