This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDS64EVM: System Analyzer support for AM64x

Part Number: TMDS64EVM

Dear TI Team,

I am trying to run the 'RTOS Analyzer' tool in CCS 12.5 to analyse the R5 core. I have the 'Simple EtherCAT Slave' sample project running on the evaluation board, which boots a FreeRTOS on the R5. I am familiar with the System Analyzer User's Guide (ti.com). As it is from 2014 and some things have changed since then (e.g. .syscfg-file instead of .cfg-file), my question is whether System Analyzer and RTOS Analyzer are compatible with the AM64x and if there is more up-to-date documentation on this.

If not: Are there any alternative ways to do a load analysis of the R5 core running a FreeRTOS?

Thanks and best regards,
Jonas