Part Number: TDA4VH-Q1
Hi,
THe datasheet gives some layout constraints relative to processor to OSPi flash interconnect (external LBCLKO to DQS loopback).
I understand that this intends to mimic the global forward + reverse electrical delay.which can be very necessary when reading at high speed burst.
1) I am wondering how this works when reading a single byte from a QSPI flash. How the Flash access time is taken into account ?
2) How should be calculated the external loopback length when the processor-to-flash interconnection is not direct but through some logic ( eg buffers, or FPGA) ?
3) I could not find where we could set the SPI clock frequency value. What are the lower and upper limits ?
With best regards,
Bruno