This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM368 boot successful using nfs but getting errors



 

 

Hi,

First of all sincere thanks to Anshuman for guiding me.

 

Now i am able to get the board boot up but i am getting the erros as given below:

 

umping to entry point at 0x81080000

U-Boot 1.3.4 (Dec  9 2010 - 17:44:14) DM368-IPNC-1.0.1

I2C:   ready
DRAM:  128 MB
NAND:  NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Bad block table found at page 65472, version 0x01
Bad block table found at page 65408, version 0x01
128 MiB
In:    serial
Out:   serial
Err:   serial
ARM Clock :- 432MHz
DDR Clock :- 340MHz
Ethernet PHY: GENERIC @ 0x01
Hit any key to stop autoboot:  0

Loading from NAND 128MiB 3,3V 8-bit, offset 0x500000
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1865336 Bytes =  1.8 MB
   Load Address: 80008000
   Entry Point:  80008000
## Booting kernel from Legacy Image at 80700000 ...
   Image Name:   Linux-2.6.18_pro500-davinci_IPNC
   Image Type:   ARM Linux Kernel Image (uncompressed)
   Data Size:    1865336 Bytes =  1.8 MB
   Load Address: 80008000
   Entry Point:  80008000
   Verifying Checksum ... OK
   Loading Kernel Image ... OK
OK

Starting kernel ...

Linux version 2.6.18_pro500-davinci_IPNC_DM368_2.6.0 (mayank@mayank-laptop) (gcc version 4.2.0 (MontaVista 4.2.0-16.0.32.0801914 2008-08-30)) #1 PREEMPT Sun1
CPU: ARM926EJ-S [41069265] revision 5 (ARMv5TEJ), cr=00053177
Machine: DaVinci DM368 IPNC
Memory policy: ECC disabled, Data cache writeback
DaVinci DM0365 variant 0x8
PLL0: fixedrate: 24000000, commonrate: 170000000, vpssrate: 340000000
PLL0: vencrate_sd: 75555555, ddrrate: 340000000 mmcsdrate: 48571428
PLL1: armrate: 432000000, voicerate: 20571428, vencrate_hd: 27000000
CPU0: D VIVT write-back cache
CPU0: I cache: 16384 bytes, associativity 4, 32 byte lines, 128 sets
CPU0: D cache: 8192 bytes, associativity 4, 32 byte lines, 64 sets
Built 1 zonelists.  Total pages: 12288
Kernel command line: mem=48M console=ttyS1,115200n8 root=/dev/mtdblock3 rw initrd=0x82000000,16M ip=192.168.1.101:192.168.1.100:192.168.1.1:255.255.255.0:::’
TI DaVinci EMAC: kernel boot params Ethernet address: 00:0C:0C:A0:00:24��’
PID hash table entries: 256 (order: 8, 1024 bytes)
Clock event device timer0_0 configured with caps set: 07
Console: colour dummy device 80x30
Dentry cache hash table entries: 8192 (order: 3, 32768 bytes)
Inode-cache hash table entries: 4096 (order: 2, 16384 bytes)
Memory: 48MB = 48MB total
Memory: 28196KB available (3193K code, 654K data, 184K init)
Security Framework v1.0.0 initialized
Capability LSM initialized
Mount-cache hash table entries: 512
CPU: Testing write buffer coherency: ok
checking if image is initramfs...it isn't (bad gzip magic numbers); looks like an initrd
Freeing initrd memory: 16384K
NET: Registered protocol family 16
DaVinci: 104 gpio irqs
MUX: initialized GPIO20
MUX: initialized I2C_SCL
Generic PHY: Registered new driver
ch0 default output "COMPOSITE", mode "NTSC"
VPBE Encoder Initialized
SCSI subsystem initialized
NET: Registered protocol family 2
IP route cache hash table entries: 512 (order: -1, 2048 bytes)
TCP established hash table entries: 2048 (order: 1, 8192 bytes)
TCP bind hash table entries: 1024 (order: 0, 4096 bytes)
TCP: Hash tables configured (established 2048 bind 1024)
TCP reno registered

 ***davinci_spi_board_init()!<6>
 ***davinci_spi_board_init_End(0)!<5>VFS: Disk quotas dquot_6.5.1
Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
squashfs: version 3.1 (2006/08/19) Phillip Lougher
JFFS2 version 2.2. (NAND) (C) 2001-2006 Red Hat, Inc.
yaffs Sep  4 2011 17:00:04 Installing.
SGI XFS with no debug enabled
Initializing Cryptographic API
io scheduler noop registered
io scheduler anticipatory registered (default)
LTT : ltt-facilities init
LTT : ltt-facility-core init in kernel
DAVINCI-WDT: DaVinci Watchdog Timer: heartbeat 60 sec
Serial: 8250/16550 driver $Revision: 1.90 $ 2 ports, IRQ sharing disabled
serial8250.0: ttyS0 at MMIO map 0x1c20000 mem 0xfbc20000 (irq = 40) is a 16550A
serial8250.0: ttyS1 at MMIO map 0x1d06000 mem 0xfbd06000 (irq = 41) is a 16550A
RAMDISK driver initialized: 1 RAM disks of 32768K size 1024 blocksize
Davinci EMAC MII Bus: probed
MAC address is 00:0C:0C:A0:00:24
TI DaVinci EMAC Linux version updated 4.0
netconsole: not configured, aborting
Linux video capture interface: v2.00
Trying to register davinci display video device.
layer=c2f08000,layer->video_dev=c2f08160
Trying to register davinci display video device.
layer=c2f1be00,layer->video_dev=c2f1bf60
davinci_init:DaVinci V4L2 Display Driver V1.0 loaded
i2c /dev entries driver
nand_davinci nand_davinci.0: Using 4-bit hardware ECC
NAND device: Manufacturer ID: 0xec, Chip ID: 0xf1 (Samsung NAND 128MiB 3,3V 8-bit)
Creating 7 MTD partitions on "nand_davinci.0":
0x00000000-0x00300000 : "bootloader"
0x00300000-0x00500000 : "params"
0x00500000-0x00700000 : "kernel"
0x00700000-0x02700000 : "filesystem"
0x02700000-0x02900000 : "data1"
0x02900000-0x02d00000 : "Calibration"
0x02d00000-0x08000000 : "data2"
nand_davinci nand_davinci.0: hardware revision: 2.3
musb_hdrc: version 6.0, cppi-dma, peripheral, debug=0
musb_hdrc musb_hdrc: No DMA interrupt line
musb_hdrc: USB Peripheral mode controller at c3866000 using DMA, IRQ 12
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: proc
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc intf: dev (254:0)
rtc_davinci_dm365 rtc_davinci_dm365.0: rtc core: registered rtc_davinci_dm365 as rtc0
davinci-mmc davinci-mmc.0: Supporting 4-bit mode
davinci-mmc davinci-mmc.0: Using DMA mode
Advanced Linux Sound Architecture Driver Version 1.0.12rc1 (Thu Jun 22 13:55:50 2006 UTC).
ASoC version 0.13.1
CQ0093 Voice Codec 0.1
asoc: cq93vc <-> davinci-vcif mapping ok
ALSA device list:
  #0: On-chip voice codec (cq93vc)
IPv4 over IPv4 tunneling driver
TCP bic registered
NET: Registered protocol family 1
NET: Registered protocol family 17
rtc_davinci_dm365 rtc_davinci_dm365.0: setting the system clock to 2000-01-01 08:05:43 (946713943)
Time: timer0_1 clocksource has been installed.
Clock event device timer0_0 configured with caps set: 08
Switched to high resolution mode on CPU 0
IP-Config: Complete:
      device=eth0, addr=192.168.1.101, mask=255.255.255.0, gw=192.168.1.1,
     host=192.168.1.101, domain=, nis-domain=(none),
     bootserver=192.168.1.100, rootserver=192.168.1.100, rootpath=
RAMDISK: Couldn't find valid RAM disk image starting at 0.
VFS: Mounted root (cramfs filesystem) readonly.
Freeing init memory: 184K
INIT: version 2.86 booting
0
mkdir: Cannot create directory `/dev/.test': Read-only file system
Starting the hotplug events dispatcher: udevd.
Synthesizing the initial hotplug events...done.
Waiting for /dev to be fully populated...done.
0
csl: disagrees about version of symbol struct_module
insmod: cannot insert `./csl.ko': Invalid module format (-1): Exec format error
drv: disagrees about version of symbol struct_module
insmod: cannot insert `./drv.ko': Invalid module format (-1): Exec format error
BusyBox v1.2.2 (2007.03.11-00:56+0000) multi-call binary

Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR

Create a special file (block, character, or pipe).

Options:
        -m      create the speccmemk: disagrees about version of symbol struct_module
ial file using the specified mode (default a=rw)

TYPEs include:
        b:      Make a block (buffered) device
        c or u: Make a character (un-buffered) device
        p:      Make a named pipe. MAJOR and MINOR are ignored for named pipes

BusyBox v1.2.2 (2007.03.11-00:56+0000) multi-call edmak: disagrees about version of symbol struct_module
binary

Usage: mknod [OPTIONS] NAME TYPE MAJOR MINOR

Create a special file (block, character, or pipe).

Options:
        -m      create the special file using the specified mode (default a=rw)

TYPEs include:
        b:      Make a block (buffered) device
        c or u: Make a character (un-buffered) device
        p:      Make a named pipe. MAJOirqk: disagrees about version of symbol struct_module
R and MINOR are ignored for named pipes

insmod: cannot insert `cmemk.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `edmak.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `irqk.ko': Invalid module format (-1): Exec fdm365mmap: disagrees about version of symbol struct_module
ormat error
insmod: cannot insert `dm365mmap.ko': Invalid module format (-1): Exec format error
Creat queue id:0
queue id:0
FileMngThread created
Creat queue id:32769
queue id:32769
queue id:32769
AlramThread created
Share memory init success
IPNC_DM368_2.6.0 (mayank@mayank-laptop) (gcc version 4.2.0 (Mon
Creat queue id:65538
queue id:65538
Starting mounting local filesystems: mount queue id:65538
Creat queue id:98307
queue id:98307

CPU is DM368
./av_server.out DM368 NTSC APPRO2A AEWB 720P H264 5000000 VBR AUTO MENUOFF &
Check_device_version : DEVICE VER = 1 !!
none on /dev/shm type tmpfs (rw,size=5M)
none on /var/run type tmpfs (rw)
none on /tmp type tmpfs (rw,sync)
Setting up networking ...rm: unable to remove `/etc/network/run': Read-only file system
ApproDrvInit: 7
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
Error: ApproDrvInit fail
SystemInit success
Schedule manager init success
Starting hotplug subsystem:
   pci    
   pci      [success]
   usb    

AVSERVER UI: Initializing.
 ERROR  (drv.c|DRV_init|31): CSL init
 ERROR  (drv.c|DRV_init|107): DRV_init()
 ERROR  (avServerApi.c|AVSERVER_init|572): DRV_init()
 ERROR  (avServerUi.c|UI_start|54): AVSERVER_init()
   usb      [success]
   isapnp 
   isapnp   [success]
   ide    
   ide      [success]
   input  
   input    [success]
   scsi   
   scsi     [success]
done.
Starting portmap daemon: portmap.
Starting internet superserver: inetdcrc_ccitt: disagrees about version of symbol struct_module
.
libcrc32c: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/crc-ccitt.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/libcrc32c.ko': Invalid module format (-1): Exec format error
deadline_iosched: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/deadline-iosched.ko': Invalid module format (-1): Exec format error
cfq_iosched: disagrees about version of symbol struct_module
i2c_emac: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/cfq-iosched.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/i2c-emac.ko': Invalid module format (-1): Exec format error
sbull: disagrees about version of symbol struct_module
crc32c: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/sbull.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/crc32c.ko': Invalid module format (-1): Exec format error
deflate: disagrees about version of symbol struct_module
des: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/deflate.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/des.ko': Invalid module format (-1): Exec format error
md5: disagrees about version of symbol struct_module
sha1: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/md5.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/sha1.ko': Invalid module format (-1): Exec format error
nls_ascii: disagrees about version of symbol struct_module
nls_utf8: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/nls_ascii.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/nls_utf8.ko': Invalid module format (-1): Exec format error
exportfs: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/exportfs.ko': Invalid module format (-1): Exec format error
nfsd: disagrees about version of symbol struct_module
loop: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/nfsd.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/loop.ko': Invalid module format (-1): Exec format error
tun: disagrees about version of symbol struct_module
slhc: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/tun.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/slhc.ko': Invalid module format (-1): Exec format error
netconsole: disagrees about version of symbol struct_module
ppp_generic: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/netconsole.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/ppp_generic.ko': Invalid module format (-1): Exec format error
ppp_synctty: disagrees about version of symbol struct_module
ppp_async: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/ppp_synctty.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/ppp_async.ko': Invalid module format (-1): Exec format error
ppp_deflate: disagrees about version of symbol struct_module
davinci_emac: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/ppp_deflate.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/davinci_emac.ko': Invalid module format (-1): Exec format error
mmc_core: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/mmc_core.ko': Invalid module format (-1): Exec format error
mmc_block: disagrees about version of symbol struct_module
davinci_mmc: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/mmc_block.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/davinci-mmc.ko': Invalid module format (-1): Exec format error
usbcore: disagrees about version of symbol struct_module
musb_hdrc: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/usbcore.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/musb_hdrc.ko': Invalid module format (-1): Exec format error
usbmon: disagrees about version of symbol struct_module
scsi_transport_iscsi: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/usbmon.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/scsi_transport_iscsi.ko': Invalid module format (-1): Exec format error
libiscsi: disagrees about version of symbol struct_module
iscsi_tcp: disagrees about version of symbol struct_module
insmod: cannot insert `/opt/ipnc/modules/libiscsi.ko': Invalid module format (-1): Exec format error
insmod: cannot insert `/opt/ipnc/modules/iscsi_tcp.ko': Invalid module format (-1): Exec format error
sbull: disagrees about version of symbol struct_module
insmod: cannot insert `sbull.ko': Invalid module format (-1): Exec format error
mkdosfs 3.0.6 (04 Oct 2009)
queue id:0
umount: /mnt/mmc: not mounted
killall: dhcpcd: no process killed
rm: cannot remove `/var/run/dhcpcd-eth0.pid': No such file or directory
net_search_gateway:eth0, 1A8C0, 0, 1
dns=192.168.1.1
net_search_gateway:eth0, 1A8C0, 0, 1
net_search_gateway:eth0, 0, FE01A8C0, 3
dns=192.168.1.1
cp: unable to open `/mnt/ramdisk/usbconf.exe': Read-only file system
cp: unable to open `/mnt/ramdisk/autorun.inf': Read-only file system
cp: unable to open `/mnt/ramdisk/NET.TXT': Read-only file system
ERROR: Module g_file_storage does not exist in /proc/modules
g_file_storage: disagrees about version of symbol struct_module
insmod: cannot insert `g_file_storage.ko': Invalid module format (-1): Exec format error
system_server/531[CPU#0]: BUG in local_bh_enable at kernel/softirq.c:196
ApproDrvInit: 3
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
ApproDrvInit: 9
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
ApproDrvInit: 8
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
ApproDrvInit: 2
ApproDrvInit: 6
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
ApproDrvInit: 10
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'
INIT: Entering runlevel: 3
CMEM Error: init: Failed to open /dev/cmem: 'No such file or directory'

MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774)

192.168.1.101 login: root


Welcome to MontaVista(R) Linux(R) Professional Edition 5.0.0 (0702774).

login[722]: root login  on `console'

# cd /opt/ipnc/
/opt/ipnc/dhcpcd/   /opt/ipnc/modules/
# cd /usr/
/usr/bin/    /usr/lib/    /usr/local/  /usr/sbin/   /usr/share/
# cd /usr/
/usr/bin/    /usr/lib/    /usr/local/  /usr/sbin/   /usr/share/
# cd /usr/share/
/usr/share/alsa/      /usr/share/udhcpc/    /usr/share/zoneinfo/
# cd /usr/share/
/usr/share/alsa/      /usr/share/udhcpc/    /usr/share/zoneinfo/
# cd /usr/share/
/usr/share/alsa/      /usr/share/udhcpc/    /usr/share/zoneinfo/
# cd /usr/share/
/usr/share/alsa/      /usr/share/udhcpc/    /usr/share/zoneinfo/
# cd /usr/share/
# ls
alsa      udhcpc    zoneinfo
# pwd
/usr/share
# ls
alsa      udhcpc    zoneinfo
#
#
#
# ls
alsa      udhcpc    zoneinfo
# ls
alsa      udhcpc    zoneinfo
# pwd
/usr/share
# ifconfig
eth0      Link encap:Ethernet  HWaddr 00:0C:0C:A0:00:24 
          inet addr:192.168.1.168  Bcast:192.168.1.255  Mask:255.255.255.0
          UP BROADCAST RUNNING MULTICAST  MTU:1500  Metric:1
          RX packets:3914 errors:0 dropped:0 overruns:0 frame:0
          TX packets:24 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:1000
          RX bytes:413763 (404.0 KiB)  TX bytes:3773 (3.6 KiB)
          Interrupt:52 Base address:0x7000

lo        Link encap:Local Loopback 
          inet addr:127.0.0.1  Mask:255.0.0.0
          UP LOOPBACK RUNNING  MTU:16436  Metric:1
          RX packets:0 errors:0 dropped:0 overruns:0 frame:0
          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0
          collisions:0 txqueuelen:0
          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)

 

The output of printenv is as follows:

bootdelay=4
baudrate=115200
setboot=setenv bootargs $(bootargs)
bootamd=nboot 0x80700000 0 0x500000;bootm
bootfile=""
ethaddr=00:0C:0C:A0:FF:FA
rootpath=/home/mayank/DM36x/ipnc/target/filesys
nfshost=10.17.8.125
filesize=DCE000
fileaddr=82000000
ipaddr=10.17.8.131
serverip=10.17.8.125
eth=00:0C:0C:A0:07:Ea
bootcmd=nboot 0x80700000 0 0x500000;bootm
bootargs=mem=48M console=ttyS1,115200n8 root=/dev/mtdblock3 rw initrd=0x82000000,16M ip=192.168.1.101:192.168.1.100:192.168.1.1:255.255.255.0:::off eth=00:0’
stdin=serial
stdout=serial
stderr=serial
ver=U-Boot 1.3.4 (Dec  9 2010 - 17:44:14) DM368-IPNC-1.0.1

Environment size: 623/131068 bytes

 

Actually I created my own uimage in release mode and the filesystem i am using is same filesystem which

i got after untarring the Appro original cramfsImage_dm368_ipnc_2.60.01 image 

I understand that because of incompatibility of uimage and cramfs image i am getting the

driver related errors.But ic ouldn't understand the solution.

Also cramfs file system is readonly so once even after mounting the filesystemon board

i cannot create any directory say in /usr/share and see the same dir on the board.

So my doubts are:

how to get rid of these errors(if we have to use some other filesystem or fs image.)

 

2.Also if someone could tell the diff b/w /dev/nfs,/dev/ram0,/dev/mtdblock3 in bootargs.

Thanks and Regards,

Mayank

 

 

  • Mayank,

    Your problem here is that your uImage version and module version do not match. As i mentioned earlier also, you should use NFS for your development work as using cramfs will need additional steps of always creating a cramfs and programming it on NAND. So just setup your NFS system and mount it as root filesystem on the target.

    The steps to get the filesystem from the released cramfs is mentioned in userguide. You can use this extracted file system as NFS exported filesystem. Once this is done, you rebuild the code. This will regenerate the cmem.ko and other kernel modules. You can then easily run the standard IPNC app once you boot your IPNC.

    MAYANK AGARWAL said:

    2.Also if someone could tell the diff b/w /dev/nfs,/dev/ram0,/dev/mtdblock3 in bootargs.

    This is a standard boot argument which tells where the kernel, where the filesystem resides.

    /dev/nfs means the root filesystem is mounted from NFS

    /dev/ram0 means the ramdisk is used as root filesystem media

    /dev/mtdblock3 means that mtdblock3 partition on the NAND is used as root filesystem media

    Hope this answers your question.

    Regards,

    Anshuman

    PS: Please mark this post as verified, if you think it has answered your question. Thanks.