Other Parts Discussed in Thread: AM1808
Hi all,
CPU is AM1808.
I would like to use a NOR flash device to store the file system.
However the address lines EMIFA_A[16..23] they are muxed with SD/MMC 0 lines, and I don't want to loose the SD/MMC port 0 in my application as a valuable interface for storing and booting purposes.
Can I switch the cpu's pins either on SD/MMC or on EMIFA depending on the current need?
In other words, can PINMUX registers be re-programmed run-time?
Regards,
Gabriele