This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIDL Inference Int8 preprocessing error

Hi , 

I am executing the inference for int8 of my model but the output is not correct when i was debugging it i found the deviation in the input layer of the model compared to fp32 where in fp32 i am getting correct output , can you u please let me knw if i need to do any addition preprocessing steps for int8 inference 

  • Hi,

    Can you please refer to our detailed documentation on accuracy debugs here : https://github.com/TexasInstruments/edgeai-tidl-tools/blob/master/docs/tidl_osr_debug.md

    We have created layer level debug specific notebook you might want to check the same here : https://github.com/kumardesappan/colab-notebooks/blob/main/ti_edgeai_tidl_tools.ipynb

  • yes i have referred the doccumentation and extracted the plots above can u please look into the clearly and let me knw for int8 inference should we change the input or preprocessing modules 

  • To understand the issue better can you able to share the jupyter notebook which has layer level plots so I can analyze the same at my end.

    You can share the notebook of same format we have shared above.

    Thanks 

  • Hi Abhilash,

    Is it possible for you to send the import/infer configs that you are using? As you mentioned there is something wrong with the input data layers itself, we can look at the inElementTypes that you are setting.

    Thanks,

    Sai

  • Also, I see you have shared multiple plots, these plots belong to which layers?

  • Hello Saideepak please find the below response 

    • The config files for both import and infe
      inFileFormat    = 1
      numFrames   = 1
      netBinFile      = "~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v5.bin"
      ioConfigFile   = "~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v5_1.bin"
      inFileFormat = 1 
      rawDataInElementType = 6
      inElementType = 2
      inData = ~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/lucid_laneDetection/inputs/Tidl_input.raw
      writeOutput = 2
      outData =   ~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/tidlInputOutputs/outputs/sample_output.bin
      writeTraceLevel = 3
      
      rence is also attached 
      modelType          = 2
      numParamBits       = 8
      inputNetFile      = "~/Documents/onnxmodel/customer_model_v6.onnx"
      outputNetFile      = "~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v5.bin"
      outputParamsFile   = "~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v5_"
      inDataNamesList = image,input_471,Gather_207_input,Mul_199_input,ones_input
      #outDataNamesList = seeds,output_dict_list,523,587,599
      numBatches=1
      inNumChannels = 3 2 1 1 1
      inHeight =  320 40 1 1 66
      inWidth  = 800 100 1 134 1
      inFileFormat = 1 
      inData = ~/TI/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/tidlInputOutputs/rawInputs/test_input3_tidl.raw
      
      
    • Our model input is image data and additional data to the layer operators  which is present in the .raw file which is shared 
    • The shared multiple plots in this forum is wrt to the input layers comparison 
    • test_input3_tidl.raw.txt
  • Hi,

    If you are planning to run the network in 8-bit, you should set the inElementType to 0/1 in the import config. Following is the list of data types that TIDL supports,

    If the data present in the inData file is in float, and you are planning to run the network in 8-bit, please set the following parameter in both import/infer files

    rawDataInElementType = 6

    inElementType = 0/1

    You can set the writeTraceLevel flag to enable the layer level traces, I suggest you first make sure the input is correctly passed on to the network. If you set this flag to a higher level (2/3), it should dump float traces (fixed point converted to float), you can now compare the input trace to the actual input file.

    Let me know if you face any issues.

    Thanks,

    Sai

  • I have followed the steps suggested and i am still facing the same issues with the input , i have added all the plots here for more analysis 

    comparision_outs.zip.txt

    modelType          = 2
    numParamBits       = 32
    numFrames = 2
    inputNetFile      = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/models/public/onnx/customer_model_v6.onnx"
    outputNetFile      = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v6_fp32.bin"
    outputParamsFile   = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v6_fp32"
    inDataNamesList = image,input_471,Gather_207_input,Mul_199_input,ones_input
    #outDataNamesList = seeds,output_dict_list,523,587,599
    numBatches=1
    inNumChannels = 3 2 1 1 1
    inHeight =  320 40 1 1 66
    inWidth  = 800 100 1 134 1
    inFileFormat = 1 
    inData = /home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/tidlInputOutputs/rawInputs/test_input_2_3_tidl.raw
    
    
    modelType          = 2
    numParamBits       = 8
    numFrames = 2
    inputNetFile      = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/models/public/onnx/customer_model_v6.onnx"
    outputNetFile      = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v6_int8.bin"
    outputParamsFile   = "/home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/ti_dl/test/testvecs/config/tidl_models/onnx/customer_mode_v6_int8_"
    inDataNamesList = image,input_471,Gather_207_input,Mul_199_input,ones_input
    #outDataNamesList = seeds,output_dict_list,523,587,599
    numBatches=1
    inNumChannels = 3 2 1 1 1
    inHeight =  320 40 1 1 66
    inWidth  = 800 100 1 134 1
    inFileFormat = 1 
    inData = /home//TI_SDK/ti-processor-sdk-rtos-j721e-evm-09_00_00_02/c7x-mma-tidl/tidlInputOutputs/rawInputs/test_input_2_3_tidl.raw
    rawDataInElementType = 6
    inElementType = 0
    
    

  • Hi Abhilash,

    Can you also share the 8-bit svg (last one you shared is float svg) and toy model if it's ready. I can look at them before call so that we can debug better.

    Thanks,

    Sai

  • customer_mode_v6_.zip

    Please find both the svg files for fp32 and int8 

  • It is not clear from the thread that which version are you using.

    can you confirm below

    1. Are you using the latest tool chain: 09_01_06_00

    https://github.com/TexasInstruments/edgeai-tidl-tools/blob/master/docs/version_compatibility_table.md

    2. Are you able to get good accuracy in INT8 mode with a known good reference run time such as ONNX run time using PTQ provided by them. see below

    https://onnxruntime.ai/docs/performance/model-optimizations/quantization.html#static-quantization

    Many times we have seen that network is not trained with good regularization and results in poor accuracy with INT8 mode so request you to confirm that by using external environment mentioned above

    Thanks,

    with Regards,

    Pramod

  • THe sdk version is 9.0 , i am not getting the any output from the int8 inference only 

  • I am not clear on what you meant by not getting any output with int8. If that is the case, then how did you get the mentioned plots in the first part of the thread. I will suggest to do below 

    1. Refer the documentation https://github.com/TexasInstruments/edgeai-tidl-tools/

    2. Use 9.1 SDK and latest tool chain (09_01_06_00) available in above repo 

    3. Make sure that you are able to run OOB examples first

    4. Then try your model

    5. If you face issue then please enable debug_level and share the traces, dumps and comparison plots

    Thanks

    Pramod

  • I also learnt that you are looking for an example

    I strongly suggest that you please go through the documentation at below link

    https://github.com/TexasInstruments/edgeai-tidl-tools

    There are several examples available for you to try out.

    https://github.com/TexasInstruments/edgeai-tidl-tools/tree/master/examples/osrt_python

    There are also google colab notebook for you to try out

    https://github.com/TexasInstruments/edgeai-tidl-tools/tree/master/examples/jupyter_notebooks/colab

    Refer below python file and you can find the dictionary of models, you can change with your model and try out 

     https://github.com/TexasInstruments/edgeai-tidl-tools/blob/master/examples/osrt_python/ort/onnxrt_ep.py

    Thanks,
    with Regards,

    pramod