main mpeg4 encode's parameters are set below, bit rate is 2Mbps and IVIDEO_RateControlPreset is CBR. when the system of DM365 starts up the mpeg4 video is normal for one hour or more long time. but mosaic occurs ater a period of time even if the capturing object is still. but the mpeg4 encoder's parameters aren't be changed at all. what happened ?