Other Parts Discussed in Thread: AM3359
Hi Team,
After starting kernel it is stucked and not loaded. How to solve this?
U-Boot 2020.01-00017-ged69b8232f-dirty (Feb 20 2024 - 10:59:19 +0530)
CPU : AM335X-GP rev 2.1
Model: TI AM3359 ICE-V2
DRAM: 256 MiB
ETH0, PRU
ETH1, PRU
WDT: Started with servicing (60s timeout)
NAND: 0 MiB
MMC: OMAP SD/MMC: 0
Loading Environment from FAT... OK
Net: eth0: ethernet@4a100000
Warning: Bootlimit (3) exceeded. Using altbootcmd.
Hit any key to stop autoboot: 0
Rollback to previous RootFs
Saving Environment to FAT... OK
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
574 bytes read in 3 ms (186.5 KiB/s)
Loaded env from uEnv.txt
Importing environment from mmc0 ...
switch to partitions #0, OK
mmc0 is current device
Scanning mmc 0:1...
switch to partitions #0, OK
mmc0 is current device
SD/MMC found on device 0
7647744 bytes read in 637 ms (11.4 MiB/s)
Starting kernel ...