This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM62A7: Dummy Key vs production key

Part Number: AM62A7

What is the definition of secure with dummy key and production key?

From one post, HS-FS device delivered without key, so no HS-FS deivce of AM62A like that of AM62x?

if select Production Key, how to select from H to R?

What is the recommandation to select which kind of device?

  • Hello,
    - "Secure with Dummy Key": HS-SE with the TI testing key pre-programmed, these're for internal use only.
    - "Secure with Production Key": HS-FS orderable by customer.
    You'll find the table in "11.1 Packaging Information" of AM62A datasheet on ordrable P/N info.
    Best,
    -Hong

  • Hong,

    #1. Is AM62A security features same as that of AM62x?

    #2. AM62x nomenclature has not variant options for dummy key and production key. so only has production key device?

    #3. from AM62A OPN table, acutally has not so many option from H to R, just two option of H and S for production key device, no other option.

  • A1. yes
    A2. yes. dummy key device is internal use ONLY
    A3. yes. the OPN table lists the currently available variants
    Best,
    -Hong