Hi Erick,
My application pipeline is
Camera -> ColorEncodingKernel(To convert YVYU to UYVY) -> LDC -> Scaler -> Preproc -> TIDL -> PostProc -> Custom_node ->Mosaic -> Display
Note: I have taken a working application and integrated custom_node at the above specified location. Also not considering the Output of postproc node as input of the custom node, and loading a extenal image in the kernel. I mean in the app_create_graph_custom_node i'm passing output of postproc but inside the custom kernel functionality i'm changing the input buffer.
In the Custom kernel the input and output images are VX_DF_IMAGE_U8 format. I'm loading a image using stbi_load functionality and using OpenGLES context to process the rest functionalities i need to perform on image. Now I need to display the image on mosaic. While trying to do that I'm facing the following error log.
p: Print performance statistics x: Exit Enter Choice: inside GLGPU kernel [MCU2_0] 54.294092 s: VX_ZONE_WARNING:[tivxCaptureSetTimeout:774] CAPTURE: WARNING: Error frame not provided using tivxCaptureRegisterErrorFrame, defaulting to waiting forever !!! width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 [MCU2_0] 54.657913 s: VX_ZONE_ERROR:[tivxKernelImgMosaicMscDrvPrepare:939] Fvid2_control Failed: Set Params inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 [MCU2_0] 55.213112 s: VX_ZONE_ERROR:[tivxKernelImgMosaicMscDrvPrepare:939] Fvid2_control Failed: Set Params inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 inside GLGPU kernel width height channels 768, 512, 3 [MCU2_0] 55.454052 s: VX_ZONE_ERROR:[tivxKernelImgMosaicMscDrvPrepare:939] Fvid2_control Failed: Set Params
I'm not sure where I'm missing. Kindly help me in resolving that. If i'm doing in a wrong way, let me know how to do the display?
Regards,
Chaitanya Prakash Uppala