Part Number: SK-AM62P-LP
Other Parts Discussed in Thread: AM62P, AM625
Hi!,
I am working with the EVM board, and I'm trying to use the Deep Sleep mode.
I've followed this step: https://software-dl.ti.com/processor-sdk-android/esd/AM62X/09_01_00/docs/devices/AM62X/android/Application_Notes_Android_Low_Power.html
I've followed these stepts: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_01_00_08/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Power_Management/pm_low_power_modes.html
I've followed these stepts: https://software-dl.ti.com/processor-sdk-linux/esd/AM62X/09_01_00_08/exports/docs/linux/Foundational_Components/Kernel/Kernel_Drivers/Power_Management/pm_wakeup_sources.html
These are the logs I get:
console:/ # rtcwake -s 10 -m mem wakeup using "mem" from /dev/rtc0 at Thu Feb 1 20:57:03 2024 [ 121.525624][ T2623] PM: suspend entry (deep) [ 121.533531][ T2623] Filesystems sync: 0.003 seconds [ 121.556552][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ctrl [ 121.560118][ T2623] remoteproc remoteproc0: stopped remote processor 79000000.r5f [ 121.564800][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 121.572372][ T2623] Freezing user space processes [ 121.579586][ T125] ueventd: LoadWithAliases was unable to load rpmsg:ti.ipc4.ping-pong [ 121.594747][ T2623] Freezing user space processes completed (elapsed 0.011 seconds) [ 121.602453][ T2623] OOM killer disabled. [ 121.606377][ T2623] Freezing remaining freezable tasks [ 121.615203][ T2623] Freezing remaining freezable tasks completed (elapsed 0.003 seconds) [ 121.623333][ T2623] printk: Suspending console(s) (use no_console_suspend to debug) [ 121.650442][ T2623] omap8250 2800000.serial: PM domain pd:146 will not be powered off [ 121.661408][ T76] android_work: sent uevent USB_STATE=DISCONNECTED [ 121.663157][ T2623] PM: suspend devices took 0.036 seconds [ 121.668897][ T2623] Disabling non-boot CPUs ... [ 121.671297][ T2623] psci: CPU1 killed (polled 0 ms) [ 121.677286][ T2623] psci: CPU2 killed (polled 0 ms) [ 121.686031][ T2623] psci: CPU3 killed (polled 0 ms) [ 121.691297][ C0] PM: pm_system_irq_wakeup: 244 triggered 2b1f0000.rtc [ 121.691378][ T2623] Enabling non-boot CPUs ... [ 121.691792][ T0] Detected VIPT I-cache on CPU1 [ 121.691862][ T0] GICv3: CPU1: found redistributor 1 region 0:0x00000000018a0000 [ 121.691928][ T0] CPU1: Booted secondary processor 0x0000000001 [0x410fd034] [ 121.693319][ T2623] CPU1 is up [ 121.693648][ T0] Detected VIPT I-cache on CPU2 [ 121.693709][ T0] GICv3: CPU2: found redistributor 2 region 0:0x00000000018c0000 [ 121.693774][ T0] CPU2: Booted secondary processor 0x0000000002 [0x410fd034] [ 121.695465][ T2623] CPU2 is up [ 121.695824][ T0] Detected VIPT I-cache on CPU3 [ 121.695890][ T0] GICv3: CPU3: found redistributor 3 region 0:0x00000000018e0000 [ 121.695961][ T0] CPU3: Booted secondary processor 0x0000000003 [0x410fd034] [ 121.698003][ T2623] CPU3 is up [ 121.698568][ T2623] ti-sci 44043000.system-controller: ti_sci_resume: wakeup source: 0x50 [ 122.195324][ T2630] usb 1-1: reset low-speed USB device number 2 using xhci-hcd [ 122.229331][ T6] android_work: sent uevent USB_STATE=CONNECTED [ 122.335423][ T6] android_work: sent uevent USB_STATE=CONFIGURED [ 122.502231][ T2623] am65-cpsw-nuss 8000000.ethernet: set new flow-id-base 19 [ 122.508045][ T2623] am65-cpsw-nuss 8000000.ethernet eth0: PHY [8000f00.mdio:00] driver [Generic PHY] (irq=POLL) [ 122.508073][ T2623] am65-cpsw-nuss 8000000.ethernet eth0: configuring for phy/rgmii-rxid link mode [ 122.512436][ T2623] am65-cpsw-nuss 8000000.ethernet eth1: PHY [8000f00.mdio:01] driver [Generic PHY] (irq=POLL) [ 122.512451][ T2623] am65-cpsw-nuss 8000000.ethernet eth1: configuring for phy/rgmii-rxid link mode [ 122.514619][ T2623] PM: resume devices took 0.728 seconds [ 122.710407][ T2623] OOM killer enabled. [ 122.714243][ T2623] Restarting tasks ... [ 122.717442][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 122.723363][ T2623] done. [ 122.731311][ T125] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 122.732269][ T2623] random: crng reseeded on system resumption [ 122.745035][ T125] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 122.763299][ T2623] Resume caused by IRQ 244, 2b1f0000.rtc [ 122.769088][ T2623] remoteproc remoteproc0: powering up 79000000.r5f [ 122.776370][ T2623] remoteproc remoteproc0: Booting fw image am62p-mcu-r5f0_0-fw, size 55272 [ 122.780118][ T125] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 122.786635][ T2623] rproc-virtio rproc-virtio.4.auto: assigned reserved memory node mcu-r5fss-dma-memory-region@9b800000 [ 122.797169][ T125] ueventd: LoadWithAliases was unable to load of:Nethernet-phyT(null) [ 122.801584][ T592] dwc3 31000000.usb: request 0000000000000000 was not queued to ep0out [ 122.801818][ T50] android_work: sent uevent USB_STATE=DISCONNECTED [ 122.804668][ T2623] virtio_rpmsg_bus virtio1: rpmsg host is online [ 122.812155][ T2640] virtio_rpmsg_bus virtio1: creating channel ti.ipc4.ping-pong addr 0xd [ 122.813285][ T607] read descriptors [ 122.813315][ T607] read strings [ 122.818606][ T125] ueventd: LoadWithAliases was unable to load platform:rproc-virtio console:/ # [ 122.820151][ T2623] rproc-virtio rproc-virtio.4.auto: registered virtio1 (type 7) [ 122.822082][ T125] ueventd: LoadWithAliases was unable to load platform:rproc-virtio [ 122.826960][ T2640] virtio_rpmsg_bus virtio1: creating channel rpmsg_chrdev addr 0xe [ 122.829855][ T125] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 122.832682][ T2623] remoteproc remoteproc0: remote processor 79000000.r5f is now up [ 122.832746][ T2623] PM: suspend exit [ 122.833163][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ctrl [ 122.836212][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 122.839110][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_ns [ 122.842045][ T125] ueventd: LoadWithAliases was unable to load virtio:d00000007v00000000 [ 122.932627][ T125] ueventd: LoadWithAliases was unable to load rpmsg:ti.ipc4.ping-pong [ 122.943994][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 122.958146][ T125] ueventd: LoadWithAliases was unable to load rpmsg:rpmsg_chrdev [ 123.851375][ T607] read descriptors [ 123.855081][ T607] read strings [ 124.797708][ T2640] android_work: sent uevent USB_STATE=CONNECTED [ 124.904231][ T2640] android_work: sent uevent USB_STATE=CONFIGURED
I can see that the screen and the peripherals such as a mouse, are disabled.
"This partially indicates that linux has finished it’s deep sleep sequence. For further confirmation, one can take a look at the TP25/PMIC_LPM_EN pin on the EVM (after programming the PMCTRL_SYS register (0x43018080) to 0x15). Here, if the pin is 3.3V when active and 0V when in deep sleep."
The test point according to the schematic is: TP46
The value es 3v3 and never changes.
Also, If I reed the register:
am62p:/ # devmem 0x43018080
0x00000010
In this question: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1310915/am625-device-not-able-to-wakeup-from-deep-sleep Anush says: "It should be done by default, but if not, a Linux Command you can run is "devmem2 0x43018080" which will read the register and "devmem2 0x43018080 w 0x15" to write to the register."
But if I write 0x15 to the register and send the device to DP, it reboots, so It does not work.
Q1: Is Deep Sleep actually working and turning things off? How could I know?
Q2: Where is set the 0x10 of the register? Should It be 0x10? (It in the Table 14-7826, page 7071 spruj83)
Thank for your response.