Hi, Dear Expert
As title description, this thread just a double check
I check datasheet, get some information as below. (Table 5-1. Device Comparison )
Part number variants with DSI 4L TX as "1" can only use the DSI0 interface for DSI functionality. DSI1* balls can still be used for CSI1 functionality.
Device is "TDA4AL88TGAALZRQ1", Does CSI-TX only supported on DSI1 pin interface in TDA4AL?
Many Thanks
Gibbs