MY SATA Disk failed to recongnize often.
WDC WD10EADX-00T 77.0 PQ: 0 ANSI: 5
1.00 TB/931 GiB
32 MB Cache.
boot info:
VFP support v0.3: implementor 41 architecture 3 part 30 variant c rev 3 omap_voltage_late_init: Voltage driver support not added smartreflex smartreflex: Driver initialized ata2: SATA link down (SStatus 0 SControl 300) mmc0: new high speed SDHC card at address e624 mmcblk0: mmc0:e624 SD08G 7.40 GiB mmcblk0: p1 p2 p3 davinci_mdio davinci_mdio.0: resetting idled controller net eth0: attached PHY driver [Generic PHY] (mii_bus:phy_addr=0:01, id=282f014) IP-Config: Complete: device=eth0, addr=192.168.10.235, mask=255.255.255.0, gw=192.168.10.1, host=dm8168, domain=, nis-domain=(none), bootserver=192.168.10.1, rootserver=192.168.10.115, rootpath= PHY: 0:01 - Link is Up - 100/Full ata1: softreset failed (device not ready) ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 300) ata1: link online but 1 devices misclassified, retrying ata1: SATA link down (SStatus 1 SControl 300) VFS: Mounted root (nfs filesystem) on device 0:14. devtmpfs: mounted Freeing init memory: 192K INIT: version 2.86 booting