Hi,
I'm using the C6726B DSP together with a couple of DACs and an ADC. For the DACs I use the ACLKX and AFSX pins and for the ADC the ACLKR and AFSR pins. I wish to run the DACs and ADC synchronous and have thus configured the McASP in synchronous mode. The transmit section works fine but the AFSR pin is quiet (it works fine as a GPIO).
Is it necessary to use asynchronous mode when using the AFSR pin? Upon reexamining the McASP datasheet it seems likely to be the case although I don't find it explicitly stated.
If I configure the transmit and receive sections with the same clock settings (and asynchronous mode) and start them at the same time is it safe to assume they will be synchronous and that the AFSR and the AFSX will be in phase?
Regards,
Tobias